LDOs with Wide Input and Output Voltage Ranges Unveiled by Microchip Technology

28V Input LDOs Deliver 150 mA Current; Support Output Voltages from 1.8 - 18V

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller and analog semiconductors, today announced the MCP1804 Low Dropout Regulators (LDOs), which deliver up to 150 mA of output current and support output voltages from 1.8 - 18V. The LDOs' input and output are stable, with 0.1 microfarads of input and output capacitance, and operate on a typical quiescent current of 50 microamperes. A shutdown function allows the output to be disabled, dropping the quiescent current to only 0.01 microamperes. The LDOs are available in a space-saving SOT-23, and thermally capable SOT-89 and SOT-223 packages, and are well-suited for applications in the industrial and consumer markets, such as security systems, wireless communication systems, cordless phones and home appliances.

Designers must often drop the voltage from existing high-voltage rails, such as 12V and 24V rails, to power subsystem circuitry. The MCP1804 LDOs' 28V input and wide output voltage range provide designers with a flexible means of doing this. Additionally, because the LDOs only require 0.1 microfarads of input and output capacitance, smaller and lower-cost ceramic capacitors can be used. The small and thermally capable package options make the LDOs ideal for space-constrained and high-power designs.

"We are pleased to expand our high-voltage LDO portfolio with the MCP1804 family," said Bryan J. Liddiard, vice president of marketing with Microchip's Analog and Interface Products Division. "The flexibility of these 28V, 150 mA devices reinforces our goal of providing the complete product solutions that our customers have come to expect."

Packaging, Pricing & Availability

The MCP1804 LDOs are available in 3-pin SOT-89 and SOT-223 packages, as well as a 5-pin SOT-89 package, for $0.50 each in 10,000-unit quantities. They are also available in a 5-pin SOT-23 package for $0.48 each in 10,000-unit quantities. Samples are available today, at http://www.microchip.com/get/400735706828704, and volume production-quantity orders can be placed at http://www.microchip.com/get/40073571712963, today.

For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at http://www.microchip.com/get/400735655324074.

About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/400735738888889.

Note: The Microchip name and logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Photo and Circuit Diagram available through editorial contact or Flickr (feel free to publish):

Photo
http://www.microchip.com/get/400915633912037

Circuit Diagram
http://www.microchip.com/get/400915653125

Tags / Keywords: Microchip, LDO, PIC, microcontroller, MCU, MCP1804, Linear Regulator, Analog

RSS Feed for Microchip Product News:
http://www.microchip.com/get/400735819560185


    Source: Microchip Technology Inc.