Microchip Technology Introduces mTouch(TM) Inductive Touch-Sensing Solutions
Robust Touch-Sense Technology Works Through Metal and Gloves; Is Unaffected By Water
CHANDLER, Ariz.--(BUSINESS WIRE)--
Microchip Technology Inc. (NASDAQ:MCHP), a leading provider of microcontroller and analog semiconductors, today announced the general availability of the mTouch(TM) Inductive Touch-Sensing Technology, as an addition to its capacitive touch-sensing solutions. Inductive touch sensing's fundamental operating principles enable it to work through a front panel such as plastic, stainless steel or aluminum. The technology also works through gloves and on surfaces that contain liquids. With the new technology, Microchip enables designers to integrate inductive touch-sensing functionality with their existing application code in a single standard 8-, 16- or 32-bit PIC(R) microcontroller (MCU) or 16-bit dsPIC(R) Digital Signal Controller (DSC), thus reducing total system costs. The technology implementation information is available for download, now, from the Microchip Touch Sensing Design Center at www.microchip.com/mtouch.
Touch sensing continues to gain traction as an alternative to traditional push-button user interfaces, which improves reliability and lowers total system costs. Touch sensing also enables a completely sealed and modern-looking design. Major applications for inductive touch-sensing user interfaces include those in the appliance market because of the possibility of a stainless steel front panel; the industrial market because of the technology's robustness; and the automotive market because of the technology's sleek aesthetics and ability to reduce accidental touch triggers.
"Microchip continues to make it easy, inexpensive and royalty-free for engineers to implement touch-sensing interfaces into their designs," said Steve Drehobl, vice president of Microchip's Security, Microcontroller and Technology Development Division. "With the addition of inductive touch technology, we now give designers even more flexibility to choose the best touch-sensing technology for their application."
Implementation details for Microchip's Inductive Touch-Sensing Solutions are available now, via a free download from Microchip's Web site at www.microchip.com/mtouch. Items available for download include:
-- User's manual with Quick-Start Guide for building an inductive
touch-sensing application
-- Application Notes covering hardware and software design
practices, with example implementations for inductive
touch-sensing solutions, such as:
1. Inductive-Touch Mechanical Design
2. Inductive-Touch Hardware
3. Inductive-Touch Software
-- Graphical User Interface software tools for analysis of
designs, utilizing Microchip's PICkit(TM) Serial Analyzer
Development Tool
-- Source Code for a variety of sensing routines
-- Frequently asked questions
For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at www.microchip.com/mtouch.
Microchip Customer Support
Microchip is committed to supporting its customers by helping design engineers develop products faster and more efficiently. Customers can access four main service areas at www.microchip.com. The Support area provides a fast way to get questions answered; the Sample area offers free evaluation samples of any Microchip device; microchipDIRECT provides 24-hour pricing, ordering, inventory and credit for convenient purchasing of all Microchip devices and development tools; finally, the Training area educates customers through webinars, sign-ups for local seminar and workshop courses, and information about the annual MASTERs events held throughout the world.
About Microchip Technology
Microchip Technology Inc. (NASDAQ:MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, dsPIC, MPLAB and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. mTouch and PICkit are trademarks of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Photos available through editorial contact
Source: Microchip Technology Inc.
Released November 11, 2008