Microchip Technology Adds More Low Pin Count Members to the World's Highest Performance 16-Bit MCU Family
PIC24H Family Additions Provide 40 MIPS Performance with up to 32 Kbytes of Flash Memory in 28- and 44-Pins; as Small as 6X6 mm Packages
CHANDLER, Ariz.--(BUSINESS WIRE)--
Microchip Technology Inc. (NASDAQ:MCHP), a leading provider of microcontroller and analog semiconductors, today announced three additions to the PIC24H high-performance 16-bit microcontroller family--featuring low pin counts with up to 32 Kbytes of Flash program memory in packages as small as 6x6 mm. These 28- and 40-pin, 40 MIPS devices start at $2.29 each in 10,000-unit quantities and are developed for cost-sensitive, space-constrained applications.
"These new 16-bit microcontroller products are a natural fit for low pin count 8-bit MCU applications that must migrate to achieve higher performance," said Sumit Mitra, vice president of Microchip's Digital Signal Controller Division. "They are also expected to be an attractive stepping stone for designers who see DSP functionality in their future and desire a platform for seamless upgrades."
Microchip is the only company to offer seamless migration among all of its 8-, 16- and 32-bit devices, including pin, peripheral, software and tool compatibility between its 16-bit and 32-bit microcontrollers and DSP-enabled DSCs. Being able to easily migrate among the more than 100 dsPIC(R) DSCs and PIC24 microcontrollers in Microchip's rapidly growing 16-bit portfolio accelerates time to market and provides a path to quickly respond to requirement changes during the design process, while providing the scalability to serve many applications.
"With their dsPIC DSCs and PIC24 MCUs, Microchip is the only company on the planet with truly unified DSP and MCU product lines," said Will Strauss, president of Forward Concepts. "The dsPIC33 family gives MCU people an easy migration path to DSP performance."
The PIC24HJ32 family also features Peripheral Pin Select, which allows designers to remap digital I/O to optimize board layout--enabling smaller boards, less noise and the use of a lower pin count microcontroller. Other key features of the new microcontroller family include:
-- 40 MIPS performance in 6x6 mm packages
-- 32 or 16 Kbytes of Flash and 2 Kbytes of RAM
-- Analog-to-Digital Converter w/ up to 13 channels, and
user-selectable 10-bit or 12-bit mode (10-bit mode enables
simultaneous sampling, eliminating lag time between samples)
-- 1 UART, 1 SPI and 1 I2C(TM) Port
Development Support
The PIC24HJ32 family is supported by the full complement of tools that are common to all of Microchip's controllers, including the free MPLAB(R) Integrated Development Environment with its Visual Device Initializer component, which graphically assists designers in mapping pins and initializing code for the on-chip Peripheral Pin Select pin-mapping function. The MPLAB C30 C compiler provides industry-leading code densities, along with math and peripheral libraries. For emulation and debugging, Microchip offers the full-featured MPLAB REAL ICE(TM) tool and the low-cost MPLAB ICD 2 tool. Finally, the 16-bit 28-pin starter board (part # DM300027) can be used for development with any of Microchip's 28-pin 16-bit microcontrollers and DSCs, while the 44-pin family members are supported with a plug-in module for the Explorer 16 Development Board (part # DM240001).
Pricing & Availability
All three members of the PIC24HJ32 family are available today for general sampling and volume production, with prices starting at $2.29 each in 10,000-unit quantities. The PIC24HJ32GP202 is available in 28-pin SDIP, SOIC and QFN packages. The PIC24HJ32GP204 and PIC24HJ16GP304 are both available in 44-pin TQFP and QFN packages. For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at www.microchip.com/16bit.
Microchip Customer Support
Microchip is committed to supporting its customers by helping design engineers develop products faster and more efficiently. Customers can access four main service areas at www.microchip.com. The Support area provides a fast way to get questions answered; the Sample area offers free evaluation samples of any Microchip device; microchipDIRECT provides 24-hour pricing, ordering, inventory and credit for convenient purchasing of all Microchip devices and development tools; finally, the Training area educates customers through webinars, sign-ups for local seminar and workshop courses, and information about the annual MASTERs events held throughout the world.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, PIC, dsPIC, and MPLAB are registered trademarks of Microchip Technology Inc. in the USA and other countries. REAL ICE is a trademark of Microchip Technology Inc. in the USA and other countries. All other trademarks mentioned herein are the property of their respective companies.
Photo and Block Diagram available through editorial contact.
Source: Microchip Technology Inc.
Released November 27, 2007