Microchip Releases 20 Advanced Wi-Fi® Products for Industrial and Commercial Applications
Company’s wireless connectivity portfolio represents one of the industry’s most extensive selection of Wi-Fi solutions and comprehensive support systems
CHANDLER, Ariz., Oct. 15, 2024 (GLOBE NEWSWIRE) -- With Industry 4.0, the rapid rise of Artificial Intelligence (AI), digitized manufacturing and the age of IoT everything, the demand for wireless connectivity in commercial and industrial applications is growing at an exceptional pace. These applications typically require reliable connectivity that can withstand extreme environments that are exposed to high temperatures, background noise and obstructions. To help meet this need, Microchip Technology (Nasdaq: MCHP) has added 20 products to its Wi-Fi® portfolio. Expanding one of the industry’s most extensive wireless connectivity product lines, Microchip offers high-performance Wi-Fi microcontrollers (MCUs), network and link controllers and plug-and-play modules designed to simplify development and speed time to market.
The company’s Wi-Fi solutions are designed to support various application needs and developer skill levels. The selection ranges from modules that are regulatory certified in several countries that require no Radio Frequency (RF) expertise and little programming to robust Systems-on-Chip (SoCs) with industrial-level features.
Microchip’s Wi-Fi portfolio includes:
- Wi-Fi MCUs: all-in-one solution designed to combine the functionality of an MCU with reliable wireless connectivity
- Link Controllers: an SDIO interface enables the addition of Wi-Fi to Linux® MPUs
- Network Controllers: an SPI interface allows the addition of wireless connectivity to an MCU
- Plug-and-Play Modules: simplify wireless-to-cloud connectivity by sending simple text commands from an MCU over a UART interface
“For decades Microchip has been a respected MCU provider, and we’ve leveraged that background, along with our comprehensive support ecosystem, to build a portfolio of Wi-Fi products and services that is unmatched in the industry today,” said Rishi Vasuki, vice president of Microchip’s wireless solutions business unit. “Our experience allows us to provide developers with wireless solutions designed to support advanced applications such as precision sensing and motor control operating under harsh conditions.”
The latest PIC32MZ-W1 Wi-Fi MCUs build on Microchip’s trusted 32-bit MCU line and feature advanced analog peripherals—including CAN, Ethernet, capacitive touch and ADC—to offer exceptional versatility. Additionally, the new devices feature some of the highest General-Purpose Input/Output (GPIO) capabilities on the market.
Also included in the lineup are next-generation WINCS02 network controllers and WILCS02 link controllers. Updates to the popular WINC and WILC solutions include improved radio performance and enhanced security features. The new wireless modules are pin-to-pin compatible with previous generations to ease migration from legacy devices.
To simplify Wi-Fi to cloud connectivity, Microchip has also expanded its plug-and-play product line with new RNWF02 modules. These modules connect MCUs to a cloud platform using simple ASCII commands sent over a UART interface.
Secure connections, which are critical for Wi-Fi applications that send or receive data from the cloud, can be challenging to implement depending on the developer’s skill level. To ease this process, Microchip has integrated its Trust Platform into many of its Wi-Fi products. Trust&GO module variants are pre-provisioned for secure authentication with popular cloud services, including AWS® and Azure®, to streamline the process of network authentication.
Millions of Microchip Wi-Fi products are already powering industrial applications around the world, offering seamless integration, enhanced security, robust connectivity and long-term performance and reliability throughout their lifecycle. To learn more, visit Microchip’s Embedded Wireless Connectivity Products web page.
Development Tools
Microchip’s Wi-Fi portfolio is supported by a comprehensive suite of development tools, application demos, evaluation boards and services. Additional services include free design checks to give developers the support they need to create high-quality products efficiently.
Pricing and Availability
For additional information or to purchase, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s Purchasing and Client Services website, www.microchipdirect.com.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: https://www.flickr.com/photos/microchiptechnology/54053054464/sizes/l/
About Microchip Technology:
Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control and processing solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve approximately 123,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, the Microchip logo, MPLAB are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
| Editorial Contact: | Reader Inquiries: |
| Amber Liptai | 1-888-624-7435 |
| 480-792-5047 | |
| amber.liptai@microchip.com |
Source: Microchip Technology Inc.
Released October 15, 2024