Industry’s First Automotive-Qualified Gen 4 PCIe® Switches Enable Autonomous Driving Ecosystem
Switchtec™ Gen 4 PCIe switches provide low-latency, low-power, and high-performance connectivity for ADAS designs
CHANDLER, Ariz., Feb. 21, 2022 (GLOBE NEWSWIRE) -- High-speed, low-latency connectivity solutions for distributed, heterogenous compute systems are a fundamental element in next-generation autonomous driving applications. Microchip Technology Inc. (Nasdaq: MCHP) is announcing the market’s first Gen 4 automotive-qualified PCIe® switches. These Switchtec™ PFX, PSX, and PAX switch solutions provide cutting-edge compute interconnect capabilities for Advanced Driver-Assistance Systems (ADAS).
“Our automotive-qualified portfolio of Switchtec Gen 4 switches provides the lowest latency and high bandwidth required to link the CPU and accelerator building blocks used in ADAS applications,” says Krishna Mallampati, associate director of marketing and applications for Microchip’s data center solutions business unit. “We are delighted to see the culmination of several years of collaboration with key technology partners and customers to bring these solutions to market.”
Switchtec Gen 4 PCIe switches provide the high-speed interconnect that supports distributed, real-time safety-critical data processing in ADAS architectures. PCIe is emerging as the preferred compute interconnect solution for the automotive industry for the same reasons it has become pervasive in the data center market. It provides ultra-low latency and low-power bandwidth scalability to CPUs and specialized accelerator devices.
“The qualification of Microchip’s solutions to meet the stringent needs of the automotive market is a significant milestone, and one NVIDIA closely collaborated on,” said Michael Truog, senior director of Automotive Platform Architecture at NVIDIA. “Microchip’s automotive PCIe switches deliver flexibility and advanced programmability, enabling high-speed SoC and GPU connectivity within our NVIDIA DRIVE platform.”
Development Tools
Microchip’s ChipLink diagnostic Graphical User Interface (GUI) provides extensive debug, diagnostics, configuration and forensics tools for rapid deployment.
Availability
Switchtec automotive-qualified Gen 4 PCIe switches are available in production. For purchasing information, contact a Microchip sales representative.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: https://www.flickr.com/photos/microchiptechnology/51870164131/sizes/l/
About Microchip Technology
Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. Switchtec is a trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks, mentioned herein are the property of their respective companies.
| Editorial Contact: | Reader Inquiries: |
| Jessica Goble | 1-888-624-7435 |
| 602-341-8743 | |
|
Jessica.goble@microchip.com |
Source: Microchip Technology Inc.
Released February 21, 2022