Microchip Expands Space-Qualified FPGA Portfolio with New RT PolarFire® Device Qualifications and SoC Availability
Latest achievements highlight over 60 years of space heritage and commitment to high-reliability, radiation-tolerant technology for next-generation satellite and avionics systems.
CHANDLER, Ariz., July 10, 2025 (GLOBE NEWSWIRE) -- Continuing to support the evolving needs of space system developers, Microchip Technology (Nasdaq: MCHP) has announced two new milestones for its Radiation-Tolerant (RT) PolarFire® technology: MIL-STD-883 Class B and QML Class Q qualification of the RT PolarFire RTPF500ZT FPGA and availability of engineering samples for the RT PolarFire System-on-Chip (SoC) FPGA. These achievements underscore the company’s more than 60 years of spaceflight heritage and its commitment to delivering highly reliable, low-power solutions for the most demanding space applications.
MIL-STD-883 Class B and Qualified Manufacturers List (QML) Class Q are industry standards that define rigorous testing and qualification processes for microelectronic components used in high-reliability applications, such as space and defense. MIL-STD-883, developed by the U.S. Department of Defense, outlines methods for environmental, mechanical and electrical testing to ensure device reliability under extreme conditions. QML Class Q, managed by the Defense Logistics Agency (DLA), certifies that manufacturers consistently produce components meeting these stringent requirements.
Unlike traditional SRAM-based FPGAs, RT PolarFire devices utilize nonvolatile technology, making them immune to configuration memory upsets caused by radiation. This eliminates the need for external mitigation measures, helping reduce system complexity and overall cost. RT PolarFire FPGAs consume up to 50% less power than mid-range SRAM-based alternatives, enabling satellite designers to optimize Size, Weight and Power (SWaP) without compromising mission-critical reliability. The PolarFire RTPF500ZT FPGA advances the family’s capabilities, offering enhanced Single Event Latch-up (SEL) radiation performance and increased robustness for inflight programming compared to the original RTPF500T.
"Microchip Technology has a proven track record of supporting critical space missions, spanning low Earth orbit, satellite platforms and deep space exploration," said Shakeel Peera, vice president of marketing and strategy for Microchip’s FPGA business unit. "Our commitment to stringent quality standards, compliance with international regulations and long-term product reliability has solidified Microchip’s reputation as a trusted provider of aerospace hardware. As the industry demands higher performance, increased logic density and robust security, we remain dedicated to innovating solutions that address the evolving needs of modern space systems."
Engineering samples of the RT PolarFire SoC FPGA further strengthen Microchip’s portfolio of space-qualified solutions. This SoC integrates a real-time, Linux®-capable, RISC-V®-based microprocessor subsystem with a flight-proven FPGA architecture, enabling both flexible software support and deterministic real-time performance. With a roadmap to QML Class V and Class Y, the RT PolarFire SoC FPGA is well suited for central satellite processing, avionics and payload control where high reliability is essential.
RT PolarFire devices are supported by the Libero® SoC Design Suite, a comprehensive IP library, reference designs and solution stacks tailored for space applications. RT PolarFire SoC FPGAs also integrate with Microchip’s Mi-V ecosystem for RISC-V development. Additionally, development kits and hardware platforms are available to facilitate rapid prototyping, hardware validation and system integration, enabling engineers to efficiently bring mission-critical space systems from concept to deployment.
Microchip’s latest milestones in radiation-tolerant FPGA technology reflect ongoing progress in addressing the stringent requirements of contemporary space missions. With a focus on continuous improvement and industry collaboration, the company is well positioned to support the next generation of satellite, avionics and deep space systems. Additional information, technical documentation, and development resources can be found on the Microchip radiation-tolerant FPGA website.
Pricing and Availability
Purchase directly from Microchip or contact a Microchip sales representative or authorized worldwide distributor.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
• Application image: https://www.flickr.com/photos/microchiptechnology/54623970661/sizes/o/
About Microchip Technology:
Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control and processing solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve over 100,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, the Microchip logo, Libero and PolarFire are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
| Editorial Contact: | Reader Inquiries: |
| Amber Liptai | 1-888-624-7435 |
| 480-792-5047 | |
| amber.liptai@microchip.com |
Source: Microchip Technology Inc.
Released July 10, 2025