Microchip and Acacia Collaborate to Enable Market Transition to 400G Pluggable Coherent Optics for Data Center Routing, Switching and Metro OTN Platforms
Solutions enable encrypted 100/400 GbE, FlexE and Flexible OTN interfaces for 400ZR, OpenZR+ and Open ROADM applications
CHANDLER, Ariz. and MAYNARD, Mass., Oct. 06, 2021 (GLOBE NEWSWIRE) -- Bandwidth growth, driven by the expansion of data centers and 5G network build-outs, is expected to drive the need for faster coherent Dense Wavelength Division Multiplexing (DWDM) pluggable optics. Consequently, Data Center Interconnect (DCI) and metro Optical Transport Network (OTN) platforms are transitioning from 100/200G to 400G pluggable coherent optical modules to support these hyper-connected architectures. Microchip Technology Inc. (Nasdaq: MCHP) and Acacia, now part of Cisco (Nasdaq: CSCO), are supporting this transition by bringing to market interoperable solution sets consisting of Microchip’s DIGI-G5 OTN processor and META-DX1 terabit secured-Ethernet PHY and Acacia’s 400G pluggable coherent optics. The purpose of the collaboration is to establish an ecosystem to support 400G CFP2-DCO, QSFP-DD and OSFP modules for the 400ZR specification as well as the OpenZR+ and Open ROADM Multi-Source Agreement (MSA) applications.
The collaboration between Microchip and Acacia helps to enable the use of 400G coherent pluggables in OTN and Ethernet systems as follows:
- For converged packet/OTN optical platforms, Microchip’s DIGI-G5 and Acacia’s 400G CFP2-DCO module are designed to enable terabit-class OTN switching line cards, muxponders, and switchponders. The DIGI-G5 interoperates with Acacia’s 400G CFP2-DCO module using a Flexible OTN (FlexO) or NxOTU4 interface to efficiently support OTN traffic, including Open ROADM MSA interface modes and 200G/400G ITU-T standards currently being drafted.
- For compact modular optical systems, Microchip’s META-DX1 and Acacia’s 400ZR and OpenZR+ modules are designed to enable 400G flexible line rate muxponders/transponders with support for multiple client optics types including QSFP28, QSFP-DD, and OSFP modules, helping service providers to transition from 100 GbE to 400 GbE using the same hardware.
- For data center routing and switching platforms, Microchip’s META-DX1 and Acacia’s 400ZR and OpenZR+ modules are designed to enable dense 400 GbE or FlexE with per port MACsec encryption coherent line cards. This helps customers leverage IP routers/switches over DWDM (IPoDWDM) infrastructure in DCI deployments.
“DIGI-G5 and META-DX1 have enabled our optical transport, IP routing and Ethernet switching customers to implement a new class of multi-terabit OTN switching and high-density 100/400 GbE and FlexE line cards that deliver on stringent packet timing and integrated security capabilities for the build out of cloud and carrier 5G-ready optical networks,” said Babak Samimi, vice president for Microchip’s Communications business unit. “Our interoperability efforts with Acacia help to demonstrate that an ecosystem for volume deployment of these new line cards with pluggable 400G coherent optics exists.”
“With Acacia’s 400G coherent modules verified to interoperate with Microchip’s DIGI-G5 and META-DX1 devices, we see it as a robust solution designed to address network capacity growth and improved efficiency,” said Markus Weber, senior director DSP, product line management of Acacia, now part of Cisco. “The compact size and power efficiency of our 400G OpenZR+ CFP2-DCO modules were designed to help network operators deploy and scale capacity of high-bandwidth DWDM connectivity between data centers and in metro networks.”
Additional Resources
For more information about the Microchip products, contact a Microchip sales representative, authorized worldwide distributor, or visit the DIGI-G5 and META-DX1 pages.
For more information on Acacia’s 400G coherent pluggable optical solutions, visit acacia-inc.com/products/.
For additional information on standards:
- For OpenZR+ MSA visit openzrplus.org
- For Open ROADM MSA visit openroadm.org
- For 400ZR visit www.oiforum.com/technical-work/hot-topics/400zr-2/
High-res images available through Flickr or editorial contact (feel free to publish):
- Press image: www.flickr.com/photos/microchiptechnology/51418894532/sizes/l/
- Applications diagram: www.flickr.com/photos/microchiptechnology/51420622505/sizes/l/
About Microchip Technology
Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
For further information:
Public Relations Contacts:
Brian Thorsen
Microchip Technology
Office: 480-792-7182
Email: brian.thorsen@microchip.com
Kelly Karr
Acacia Communications
Office: 408-718-9350
Email: PR@acacia-inc.com
Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. The Cisco name and logo and the Cisco logo are registered trademarks of Cisco in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Source: Microchip Technology Incorporated
Released October 6, 2021