First Cryptographic Companion Device Brings Pre-programmed Security to the Automotive Market

Microchip’s new TrustAnchor device provides OEMs and their module suppliers with a simplified path to automotive network security, reducing costs and time to market

CHANDLER, Ariz., Nov. 11, 2020 (GLOBE NEWSWIRE) -- Due to the rise of in-vehicle network connections like Bluetooth® and LTE/5G, today's vehicles host more vulnerabilities than ever before, driving new cybersecurity regulations and specifications for the automotive market. Helping OEMs and their module suppliers simplify the upgrade of existing designs to meet security requirements for future generations, Microchip Technology Inc. (Nasdaq: MCHP) today announced its CryptoAutomotive™ security IC, the TrustAnchor100 (TA100). The cryptographic companion device supports in-vehicle network security solutions such as secure boot, firmware update and message authentication, including Controller Area Network (CAN) MAC at bus speed. 

In order to comply with the new security specifications, automotive designers must rearchitect the vehicle’s electronic control units (ECUs) with secure hardware. Existing solutions in the market include single chip dual core hardware security module (HSM) devices, which require OEMs and their module suppliers to rearchitect their application software to integrate security. In addition to the effort required for this integration, the risk of security holes introduced in disparate implementations pose significant barriers through this path. Third party security software can help overcome this barrier in part with increasing development costs.

The TA100 provides an alternative in-vehicle network architecture implementation for secure boot and message authentication — and has already been approved by multiple OEMs around the world as a solution for EVITA Medium and EVITA Full HSM requirements. Its feature set was designed based on careful review of several prominent OEM cybersecurity specifications to help facilitate a Tier 1’s pursuit of OEM Part Production Approval (PPAP). Additionally, Microchip offers security specification and Request for Quote (RFQ) review services to assist Tier 1s in developing educated responses, improving their project award success rate. The TA100 removes the challenges associated with secure code development and provisioning by offering pre-programmed cryptographic internal application code provisioned with unique asymmetric key-pairs and associated x.509 certificates — reducing risk, cost and time to market.

The device is confirmed with high resistance to attack through intensive third-party vulnerability assessments. It is AEC-Q100 Automotive Grade-1 qualified, FIPS 140-2 CMVP Security Level 2 rated and Physical Key Protection Level 3 certified, and it has achieved the highest possible vulnerability assessment rating of Joint Interpretation Library (JIL) High. In addition, the TA100 provides software components like AUTOSAR drivers, MCALs and Microchip’s CryptoAuthentication™ library that allow seamless integration into the industry standard operating system, AUTOSAR, or customized software stacks for crypto functions.

“The TrustAnchor100 provides relief for automotive Tier 1s and OEMs when upgrading thousands of ECUs with security,” said Nuri Dagdeviren, vice president of Microchip’s secure products group. “Combining the TA100 and an integrated software stack provides production ready software for our customers, enabling them to easily add security to any automotive module.”

Development Tools
The TA100 offers AUTOSAR compliant MCAL drivers that can be integrated into an AUTOSAR software stack. A full AUTOSAR reference stack is available, enabling automotive vendors to deploy the latest crypto standards into their automotive systems within standard automotive production environments. MikroBUS™ compatible socket boards are also available.

Pricing and Availability
The TA100 is available in an 8- and 14-pin SOIC packages starting at $1.50 in 10,000-unit quantities.

For additional information, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s website. To purchase products mentioned here, click to order now or contact a Microchip authorized distributor.

Resources
High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip Technology
Microchip Technology Inc. is a leading provider of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 120,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Note: The Microchip name and logo and the Microchip logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. CryptoAuthentication and CryptoAutomotive are trademarks of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact:
Chelsey Kruger
480-792-5047
chelsey.kruger@microchip.com
                Reader Inquiries:
1-888-624-7435
     

Primary Logo

Source: Microchip Technology Inc.