Accelerate Smart Embedded Vision Designs with Microchip's Expanding Low-Power FPGA Video and Image Processing Solutions
Smart Embedded Vision initiative addresses the growing need for high-speed imaging solutions to enable edge intelligence in low-power, small form factor systems
CHANDLER, Ariz., July 15, 2019 /PRNewswire/ -- As compute-intensive, vision-based systems are increasingly integrated at the network edge, Field Programmable Gate Arrays (FPGAs) are quickly becoming a preferred flexible platform for next-generation designs. In addition to requiring high bandwidth processing capabilities, these intelligent systems are deployed in small form factors with tight thermal and power constraints. To help developers accelerate designs, Microchip Technology Inc. (Nasdaq: MCHP), via its Microsemi subsidiary, today announced its Smart Embedded Vision initiative that provides solutions for designing intelligent machine vision systems with Microchip's low-power PolarFire® FPGAs. With today's announcement, Microchip extends its high-resolution smart embedded vision FPGA offerings with new enhanced high-speed imaging interfaces, an intellectual property (IP) bundle for image processing and an expanded partner ecosystem.

The Smart Embedded Vision initiative provides a suite of FPGA offerings that includes IP, hardware and tools for low-power, small form factor machine vision designs across the industrial, medical, broadcast, automotive, aerospace and defense markets. With the launch of the initiative, Microchip has added the following to further address design requirements for intelligent vision systems:
- Serial Digital Interface (SDI) IP - Used to transport uncompressed video data streams over coaxial cabling, this interface comes in multiple speeds: HD-SDI (1.485 Gbps, 720p, 1080i), 3G-SDI (2.970 Gbps, 1080p60), 6G-SDI (5.94 Gbps, 2Kp30) and 12G-SDI (11.88 Gbps, 2Kp60).
- 1.5 Gbps per lane MIPI-CSI-2 IP – Typically used in industrial cameras, MIPI-CSI-2 is a sensor interface that links image sensors to FPGAs. The PolarFire family supports receive speeds up to 1.5 Gbps per lane and transmit speeds up to 1 Gbps per lane.
- 2.3 Gbps per lane SLVS-EC Rx – SLVS-EC Rx is an image sensor interface IP supporting high-resolution cameras. Customers can implement a two-lane or eight-lane SLVS-EC Rx FPGA core.
- Multi-rate Gigabit MAC - The PolarFire family can support 1, 2.5, 5 and 10 Gbps speeds over an Ethernet PHY, enabling the initiative to meet the need for Universal Serial 10 GE Media Independent Interface (USXGMII) MAC IP with auto-negotiation.
- 6.25 Gbps CoaXPress v1.1 Host and Device IP – CoaXPress is a standard used in high performance machine vision, medical and in industrial inspection. Aligned with the industry's roadmap for the standard, Microchip will support CoaXPress v2.0, which doubles the bandwidth to 12.5 Gbps.
- HDMI 2.0b - The HDMI IP core today supports resolutions up to 4K at 60 fps transmit and 1080p at 60 fps receive.
- PolarFire FPGA Imaging IP bundle - Features the MIPI-CSI-2 and includes image processing IPs for edge detection, alpha blending and image enhancement for color, brightness and contrast adjustments.
- Expanded Partner Ecosystem – The Smart Embedded Vision initiative introduces Kaya Instruments – which provides PolarFire FPGA IP Cores for CoaXPress v2.0 and 10 GigE vision – to Microchip's partner ecosystem. The ecosystem also includes Alma Technology, Bitec and artificial intelligence partner ASIC Design Services, which provides a Core Deep Learning (CDL) framework that enables a power-efficient Convolutional Neural Network (CNN)-based imaging and video platform for embedded and edge computing applications.
"Providing a suite of IP and hardware offerings alongside our partner ecosystem is essential to our clients' ability to innovate while meeting their production schedules," said Shakeel Peera, vice president of product marketing for the FPGA business unit at Microchip's Microsemi subsidiary. "This is especially important because of the rapid evolution of machine and computer vision, driven by the growing adoption of AI, and the need to democratize edge-based vision systems."
PolarFire FPGAs offer 30 to 50 percent lower total power over competing Static Random-Access Memory (SRAM)-based mid-range FPGAs. With family members ranging from 100K to 500K logic elements (LEs), they provide five to 10 times lower static power, making them ideal for a new range of compute-intensive edge devices, including those deployed in thermally- and power-constrained environments.
Development Tools
In addition to new high-speed imaging IP cores and the PolarFire Imaging IP bundle, a new MIPI-CSI2-based machine learning camera reference design is available for smart embedded system implementations. Based on the PolarFire FPGA imaging and video kit that uses inference algorithms from Microchip partner ASIC Design Services, the reference design is free for customers to evaluate. All Smart Embedded Vision solutions are supported by the Libero® SoC Design Suite, Microchip's comprehensive development tool.
Pricing and Availability
Available through the Libero® SoC Design Suite, all IP can be implemented on the PolarFire FPGA Video and Imaging Kit, the evaluation platform for Smart Embedded Vision designs. The following IP cores are available today:
- HD-SDI (1.485 Gbps, 720p, 1080i)
- 3G-SDI (2.970Gbps, 1080p60)
- MIPI-CSI-2
- Two-lane SLVS-EC Rx FPGA core
- 6.25 Gbps CoaXPress v1.1
- HDMI 2.0 4k at 60 fps transmit and 1080p at 60 fps receive
The following IP cores will be added progressively, with all cores supported by the end of 2019:
- · 6G-SDI (5.94 Gbps, 2Kp30)
- · 12G-SDI (11.88 Gbps, 2Kp60)
- · USXGMII MAC
- · Eight-lane SLVS-EC Rx
- · 6.25 Gbps CoaXPress v2.0
- · HDMI 2.0b 4K at 60 fps receive
PolarFire Imaging IP Bundle is available for $1,499 and the MPF300-VIDEO-KIT is available for $999. For more information and to purchase products mentioned here, visit or contact sales.support@microsemi.com.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: https://www.flickr.com/photos/microchiptechnology/48235021452
About Microchip Technology
Microchip Technology Inc. is a leading semiconductor supplier of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company's solutions serve more than 125,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, the Microchip logo, PolarFire and Libero are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

View original content to download multimedia:http://www.prnewswire.com/news-releases/accelerate-smart-embedded-vision-designs-with-microchips-expanding-low-power-fpga-video-and-image-processing-solutions-300883060.html
SOURCE Microchip Technology Inc.
Released July 15, 2019