Reduce Production Costs and Time to Market with Industry’s First NOR Flash Memory Devices Featuring Embedded MAC Addresses

With no minimum order requirement, Microchip’s new family of memory devices offers pre-programmed MAC addresses for companies of all sizes

CHANDLER, Ariz., July 11, 2019 (GLOBE NEWSWIRE) -- With the rapid growth of the Internet of Things (IoT), embedded system designers must currently source, program and serialize Media Access Control (MAC) addresses from the IEEE-Registration Authority (RA) for all connected products. Only sold from the IEEE-RA in blocks ranging from 4,000 to 16 million, small-to medium-size businesses are left to pay higher costs for low-volume services. Helping eliminate the need to self-procure and manage these unique identifiers from the IEEE-RA, Microchip Technology Inc. (Nasdaq: MCHP) today introduced the SST26VF Serial Quad I/O™ (SQI™) 3V Flash family— the industry’s first NOR Flash devices to offer integrated MAC address options. Pre-programmed with EUI-48™ and EUI-64™ addresses, the devices do not have a minimum order requirement, providing cost-effective, plug-and-play storage solutions for connected applications that use Ethernet, Bluetooth®, Wi-Fi®, IEEE 802.15.4 and FireWire®.

Both the EUI-48 and EUI-64 node addresses consist of an Organizational Unique Identifier (OUI) and an Extension Identifier (EI). While the OUI is purchased from the IEEE by individual companies, the EI is assigned and managed through each company by building a unique EI into every product, thereby ensuring a globally unique Extended Unique Identifier (EUI) node address for every device used or shipped. Microchip’s pre-programmed SST26VF family of devices are flexible MAC address chips that come with uniquely pre-programmed EUI-48 addresses and compatible EUI-64 addresses — helping designers save time and costs while accelerating time to market for low-to mid-sized volume production. MAC address options are available at Flash densities of 16 megabit (Mb), 32Mb and 64Mb.

The SST26VF064BEUI, SST26VF032BEUI and SST26VF016BEUI devices feature a six-wire, 4-bit I/O interface, allowing for low-power and high-performance operation in a low pin-count package. Available in 8-pin SOIC and 8-contact WSON packages, the devices occupy less board space and lower overall system costs. They feature rich SQI flash, with flexible write-protected functionality to ensure code cannot be inadvertently over-written or erased. Integrated with Microchip’s proprietary SuperFlash® technology, the family offers high endurance, low operating currents and low power draw, making these devices ideally suited for industrial and consumer cloud-connected applications, such as smart hubs for homes, smart home appliances, building control equipment, factory automation, security and surveillance equipment.

“Following the success of Microchip’s pre-programmed MAC address and unique ID EEPROMs, we are now expanding the embedded product option into our SuperFlash® memory product line,” said Randy Drwinga, vice president of Microchip’s memory products division. “Combined with our broad lineup of microcontrollers, wired and wireless offerings and pre-programming services, the SST26VF family offers a complete turnkey solution for today’s IoT designers.”

Development Tools
Microchip offers pre-programming services for customer firmware.

Pricing and Availability
The SST26VF064BEUI is available for $2.37, the SST26VF032BEUI is available for $1.46 and the SST26VF016BEUI is available for $1.13, each in 10,000-unit quantities.

For additional information, contact a Microchip sales representative, authorized worldwide distributor or visit Microchip’s website. To sample products mentioned here visit www.microchip.com/samples. To purchase products mentioned here visit our purchasing portal.

Resources
High-res images available through Flickr or editorial contact (feel free to publish):

About Microchip Technology
Microchip Technology Inc. is a leading semiconductor supplier of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company’s solutions serve more than 125,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.

Note: The Microchip name and logo, the Microchip logo and SuperFlash are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. MiWi, Serial Quad I/O and SQI are trademarks of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Editorial Contact: Reader Inquiries:
Chelsey Kruger 1-888-624-7435
1-480-792-5047  
chelsey.kruger@microchip.com  

 

Primary Logo

Source: Microchip Technology Inc.