Industry's First Terabit-Scale Ethernet PHY Enables Highest-Density 400 GbE and FlexE Connectivity
META-DX1 uniquely combines 100 GbE, 400 GbE, FlexE, nanosecond timestamping accuracy and MACsec security engine in a single chip with terabit capacity
CHANDLER, Ariz., May 29, 2019 /PRNewswire/ -- As cloud and telecom service providers build out their networks, they need routing and switching platforms that enable them to reduce costs, optimize bandwidth and increase capacity, security and flexibility. Microchip Technology Inc. (Nasdaq: MCHP), via its Microsemi subsidiary, is the first to enable this unique set of capabilities with its META-DX1 family of Ethernet Physical-Layer (PHY) devices that integrates, onto a single chip, Ethernet ports from 1 Gigabit Ethernet (GbE) to 400 GbE, flexible Ethernet (FlexE), Media Access Control Security (MACsec) link encryption and nanosecond timestamping accuracy at terabit capacity.

The industry is transitioning from 100 Gigabit Ethernet (GbE) to 400 GbE to support traffic within hyperscale data centers. According to Cisco's Global Cloud Index, this traffic will quadruple by 2021 with data center to data center traffic growing at more than a 30 percent Cumulative Annual Growth Rate (CAGR). The META-DX1 enables line cards to quadruple in capacity – from 3.6 terabits per second (Tbps) to 14.4 Tbps with 36 ports of 400 GbE or 144 ports of 100 GbE – while supporting key features needed by service providers.
The META-DX1 MACsec engine secures traffic leaving the data center or enterprise premises, and FlexE enables both cloud and telecom service providers to meet capacity requirements while reducing fiber plant capital expenditures by optimally configuring links beyond today's fixed-rate Ethernet so they can use low-cost, high-volume optics. The META-DX1 family uniquely combines MACsec and FlexE into one solution to meet the next phase of capacity scaling in data center interconnect (DCI) buildouts. Further differentiating META-DX1, its integrated flexible crosspoint switching capability makes it easier for OEMs to navigate the market transition from 25 Gbps NRZ and 56 Gbps PAM-based architectures by enabling them to support a single design or SKU for both 100 GbE (QSFP28) and 400 GbE (QSFP-DD) optics. By providing high-performance timestamping with nanosecond-level accuracy on every port, META-DX1 also ensures network buildouts will meet the challenging timing requirements of 5G mobile base station deployments.
"The industry foresaw challenges and limitations with traditional fixed-rate Ethernet MACs when scaling data-center interconnects, and it created FlexE as a solution," said Bob Wheeler, principal analyst for networking at The Linley Group. "Microchip's META-DX1 is an integral element, enabling FlexE on data-center routers so that cloud service providers can maximize inter-data-center fiber capacity while simplifying network operations and management."
"The META-DX1 family was purpose-built to unify into a single hardware and software offering the broad range of capabilities service providers need in their network buildouts that connect enterprise and data center services to the cloud and emerging 5G applications," said Babak Samimi, vice president for Microchip's Communications business unit. "By delivering the highest-density Ethernet ports coupled with MACsec, FlexE and the nanosecond packet timing performance needed for 5G, we've introduced an innovative Ethernet connectivity platform for telecom and cloud service provider routers and switches, as well as optical transport equipment."
Product Availability
Initial META-DX1 family members will sample during the third calendar quarter of 2019. All are hardware-compatible and supported by the same Software Developer's Kit (SDK). For additional information visit the META-DX1 webpage or contact a Microchip sales representative.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Application image: https://www.flickr.com/photos/microchiptechnology/47924971123
- Chip image: https://www.flickr.com/photos/microchiptechnology/47924987693
- Video available through YouTube (feel free to post): https://youtu.be/pMEU0sIFhjY
About Microchip Technology
Microchip Technology Inc. is a leading semiconductor supplier of smart, connected and secure embedded control solutions. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company's solutions serve more than 125,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, and the Microchip logo, are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

View original content to download multimedia:http://www.prnewswire.com/news-releases/industrys-first-terabit-scale-ethernet-phy-enables-highest-density-400-gbe-and-flexe-connectivity-300857753.html
SOURCE Microchip Technology Inc.
Released May 29, 2019