Development Kit for Amazon AVS Supports Far-field Voice Interaction with Multiple Microphone Array Options
Leading audio front-end solution with one, two and three mic configurations reduces bill of materials and addresses small-form-factor designs
CHANDLER, Ariz., Jan. 8, 2019 /PRNewswire/ -- From wearables to smart lighting, voice control is increasingly becoming consumers' preferred way to interact with electronics. As developers build products of various sizes and designs to meet consumer demand, they often have trouble scaling to meet different Bill of Materials (BOM) and form factor requirements in end applications. Microchip Technology Inc. (Nasdaq: MCHP), via its Microsemi Corporation subsidiary, today announced that its AcuEdge™ ZLK38AVS Development Kit for Amazon Alexa Voice Service (AVS) now introduces far-field voice pick up and the flexibility to build devices with multiple mic array configurations. The solution reduces BOM costs while addressing the requirements of small-form-factor designs.

As a leading audio front-end development kit with one-mic hands-free and two or three-mic far-field configurations qualified by Amazon, the solution features the ZL38063 audio processor which includes a 300 MHz DSP and dedicated hardware accelerators for voice processing. It also features Stereo Acoustic Echo Cancellation (AEC), which enables barge-in recognition to improve the consumer experience in extreme audio playback environments.
With the flexibility to work with a variety of microphone options and configurations, Original Design Manufacturers (ODMs) and third-party developers can use the development kit to cost effectively achieve their design criteria across a range of applications and form-factor constraints. Available microphone configurations include:
- One-mic configuration – Offers hands-free voice coverage for products where form-factor or cost constraints preclude the use of a multi-microphone array.
- Two and three-mic linear (180-degree) configurations – Designed for sound bars, smart plugs and switches, set-top-boxes or other applications typically positioned against a wall that benefit from 180-degree far-field coverage.
- Three-mic triangular (360-degree) configuration – Also with far-field coverage qualified by Amazon, this configuration is well suited for applications that may require user interaction from any direction such as portable speakers, wide-angle IP cameras and voice-enabled Wi-Fi® routers.
The development kit enables far-field speech recognition in the presence of interfering noise sources, including device playback and external noise sources. The field-programmable, field-upgradable solution features signal processing algorithms proven to improve both local trigger detection performance and cloud speech recognition accuracy, while the multi-microphone configurations include Direction of Arrival (DOA) estimation to indicate where the primary voice sound source is located.
"Voice-enabled devices have become immensely popular and continue to gain traction in a variety of end-applications, from home automation controllers to set-top boxes," said Steve Caldwell, vice president of Microchip's Wireless Solutions Group. "The ZLK38AVS Development Kit provides the flexibility required to scale the audio front end across products lines while enabling exceptional performance in adverse audio environments."
Development Tools
The development kit includes a ZL38063 audio processor that connects directly to a Raspberry Pi® 3B with plastics and mounting hardware to simulate a typical, recommended end-application mic-speaker arrangement. It supports all microphone options and includes an LED ring to report the detected sound location, as well as a high-quality speaker that is representative of a typical smart speaker application. Microchip has audio labs and tuning facilities located worldwide that support customers from design through Amazon certification.
Pricing and Availability
The ZLK38AVS Development Kit for Amazon AVS is available today for $299. For additional information, contact a Microchip sales representative or visit Microsemi's website.
Resources
High-res images available through Flickr or editorial contact (feel free to publish):
- Development kit image: https://www.flickr.com/photos/microchiptechnology/32537747568/
About Microchip Technology
Microchip Technology Inc. is a leading provider of microcontroller, analog, FPGA, connectivity and power management semiconductors. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company's solutions serve more than 130,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, and the Microchip logo, are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

View original content to download multimedia:http://www.prnewswire.com/news-releases/development-kit-for-amazon-avs-supports-far-field-voice-interaction-with-multiple-microphone-array-options-300774376.html
SOURCE Microchip Technology Inc.
Released January 8, 2019