Industry's First RISC-V SoC FPGA Architecture Brings Real-Time to Linux, Giving Developers the Freedom to Innovate in Low-Power, Secure and Reliable Designs
Demonstrations at RISC-V Summit Dec. 4-5 to Show Size, Power and Performance Benefits of Integrating PolarFire SoC's Hard CPU Subsystem with Programmable Logic
SANTA CLARA, Calif., Dec. 4, 2018 /PRNewswire/ -- RISC-V Summit - In a new era of computing driven by the convergence of 5G, machine learning and the internet of things (IoT), embedded developers need the richness of Linux-based operating systems. These must meet deterministic system requirements in ever lower power, thermally constrained design environments—all while addressing critical security and reliability requirements. Traditional system-on-chip (SoC) field programmable gate arrays (FPGAs) blending reconfigurable hardware with Linux-capable processing on a single chip provide developers ideal devices for customization, yet consume too much power, lack proven levels of security and reliability, or use inflexible and expensive processing architectures. In response, Microchip Technology Inc. (Nasdaq: MCHP), via its Microsemi Corporation subsidiary, today extended its Mi-V ecosystem by unveiling the architecture for a new class of SoC FPGAs that combine the industry's lowest power mid-range PolarFire™ FPGA family with a complete microprocessor subsystem based on the open, royalty-free RISC-V instruction set architecture (ISA).

Announced today at the RISC-V Summit in Santa Clara, California, Microchip's new PolarFire SoC architecture brings real-time deterministic asymmetric multiprocessing (AMP) capability to Linux platforms in a multi-core coherent central processing unit (CPU) cluster. The PolarFire SoC architecture, developed in collaboration with SiFive, features a flexible 2 MB L2 memory subsystem that can be configured as a cache, scratchpad or a direct access memory. This allows designers to implement deterministic real-time embedded applications simultaneously with a rich operating system for a variety of thermal and space constrained applications in collaborative, networked IoT systems.
"The PolarFire SoC architecture is a compelling combination of low power, security and reliability in a configurable device that brings real-time to Linux," said Bruce Weyer, vice president of the Programmable Solutions business unit at Microchip. "Coupled with our robust Mi-V RISC-V ecosystem and Microchip's extensive portfolio of system solutions, the PolarFire SoC architecture gives customers an excellent platform to meet computing's next great challenges."
PolarFire SoC includes extensive debug capabilities including instruction trace, 50 breakpoints, passive run-time configurable Advanced eXtensible Interface (AXI) bus monitors and FPGA fabric monitors, and Microchip's built-in two-channel logic analyzer SmartDebug. The PolarFire SoC architecture includes reliability and security features such as single error correction and double error detection (SEC-DED) on all memories, physical memory protection, a differential power analysis (DPA) safe crypto core, defense-grade secure boot and 128Kb flash boot memory.
"As a fully customizable, programmable RISC-V platform, the PolarFire SoC architecture gives designers the freedom to create innovative Linux-based SoCs in novel and interesting ways tailored for their distinct, domain-specific requirements," said SiFive CEO Naveed Sherwami. "By leveraging SiFive's market-leading U54-MC CPU core complex, PolarFire SoC will enable designers to overcome the universal challenge of building real-time systems with predictable behaviors."
Development Tools
Evaluate and begin PolarFire SoC designs today using the antmicro Renode™ system modeling platform, which is now integrated with Microchip's SoftConsole integrated design environment (IDE) for embedded designs targeting PolarFire SoCs. A PolarFire SoC development kit is also available now, consisting of the PolarFire FPGA-enabled HiFive Unleashed Expansion Board and SiFive's HiFive Unleashed Development Board with its RISC-V microprocessor subsystem. For more information, visit www.microsemi.com/polarfiresoc or contact sales.support@microsemi.com.
Microchip's New Mi-V Embedded Experts Program
As part of today's announcement, Microchip is launching a new Mi-V Embedded Experts Program, a worldwide partner network to assist customers in hardware/software designs for PolarFire SoC. The addition of this program ensures support throughout the entire lifecycle of customer products, and helps to jump-start designs and shorten time to market. Members also get access to direct technical support and early access to development platforms and silicon. Visit www.microsemi.com/product-directory/fpga-soc/5210-mi-v-embedded-ecosystem or contact Mi-V-EmbeddedPartner@microchip.com for more information.
About Microchip
Microchip Technology Inc. is a leading provider of microcontroller, analog, FPGA, connectivity and power management semiconductors. Its easy-to-use development tools and comprehensive product portfolio enable customers to create optimal designs which reduce risk while lowering total system cost and time to market. The company's solutions serve more than 130,000 customers across the industrial, automotive, consumer, aerospace and defense, communications and computing markets. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at www.microchip.com.
Note: The Microchip name and logo, the Microchip logo and Microsemi are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. PolarFire is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

View original content to download multimedia:http://www.prnewswire.com/news-releases/industrys-first-risc-v-soc-fpga-architecture-brings-real-time-to-linux-giving-developers-the-freedom-to-innovate-in-low-power-secure-and-reliable-designs-300759560.html
SOURCE Microchip Technology Inc.
Released December 4, 2018