Microsemi RTG4 FPGAs Become Industry's First High-Speed Signal Processing Radiation-Tolerant FPGAs to Achieve QML Class V Qualification
Designation Enables Space Customers to Leverage RTG4 FPGAs' Easy Prototyping and Fast Design Times
ALISO VIEJO, Calif., Aug. 28, 2018 /PRNewswire/ -- Microsemi Corporation, a wholly owned subsidiary of Microchip Technology Inc. (Nasdaq: MCHP), today announced its RTG4™ high-speed signal processing radiation-tolerant field programmable gate arrays (FPGAs) have achieved Qualified Manufacturers List (QML) Class V qualification by the Defense Logistics Agency (DLA). The designation, the highest level of qualification for space components and a necessary step to satisfy mission assurance requirements on many space programs, opens the door for Microsemi's RTG4 FPGAs to be used on the most critical space missions with the highest standards for quality and reliability.

As the first and only radiation-tolerant FPGA offering more than 150,000 logic elements to achieve a QML Class V qualification, Microsemi's RTG4 FPGAs can now be used by developers in Class 1 space flight systems, bringing the cost and schedule advantages of FPGAs to the most demanding space missions. Many space programs are constrained to use these Class V-qualified components due to the need for the highest level of quality and reliability, and until now have been unable to use a high-speed radiation-tolerant FPGA in their signal processing systems. RTG4 FPGAs now fill this void in the marketplace, providing more signal processing bandwidth than has been previously available in radiation-tolerant non-volatile FPGAs and enabling designers of satellite on-board data processing systems to take advantage of the easy prototyping and fast design cycle times FPGAs provide.
"We believe it's critical to support our customers with the availability of our flagship radiation-tolerant FPGAs qualified to the stringent QML Class V standard—the highest qualification level for integrated circuits operating in space," said Minh Nguyen, Microsemi's senior marketing manager of space and aviation. "This designation is the culmination of hundreds of thousands of testing hours, and underscores the high reliability of these unique devices as well as our team's deep experience in developing radiation-tolerant FPGAs with industry-leading flight heritage."
Granted by the DLA, NASA and the U.S. Air Force Space and Missile Command (represented by The Aerospace Corporation), the QML Class V qualification is a strong endorsement by recognized subject matter experts on the quality and reliability of RTG4 FPGAs. This validation is increasingly important as a growing number of satellites are being built to perform a wide variety of missions, including imaging, communications, navigation, science and monitoring of weather, climate and natural resources. Many of these systems require the highest level of component quality, particularly when large revenue streams depend upon the satellites functioning correctly, or when there are national security considerations.
Microsemi's new QML Class V qualification adds to the existing designations the RTG4 FPGAs have achieved, including QML Class Q and MIL-STD-883 Class B qualifications. Details can be found in the company's reliability report, as well as its DLA Cross Reference Guide. As the company is already a QML-V certified manufacturer of high reliability FPGAs for space applications, achieving the recent additional qualification for its RTG4 FPGAs further strengthens its leadership position in the market and reflects the company's focus on developing innovative solutions to meet the increasing demands of modern satellite payloads. In addition to satellites, its RTG4 FPGAs are ideally suited for applications including space launch vehicles, planetary orbiters and landers, and deep space probes.
Leveraging Microsemi's 60-year legacy of innovation in the space market, its RTG4 devices are the latest development in a long history of radiation-tolerant FPGAs found in many NASA and international space programs. For more information, visit http://www.microsemi.com/products/fpga-soc/radtolerant-fpgas/rtg4.
About Microsemi
Microsemi Corporation, a wholly owned subsidiary of Microchip Technology, Inc. (Nasdaq: MCHP), offers a comprehensive portfolio of semiconductor and system solutions for aerospace & defense, communications, data center and industrial markets. Products include high-performance and radiation-hardened analog mixed-signal integrated circuits, FPGAs, SoCs and ASICs; power management products; timing and synchronization devices and precise time solutions, setting the world's standard for time; voice processing devices; RF solutions; discrete components; enterprise storage and communication solutions, security technologies and scalable anti-tamper products; Ethernet solutions; Power-over-Ethernet ICs and midspans; as well as custom design capabilities and services. Microsemi is headquartered in Aliso Viejo, California. Learn more at www.microsemi.com.
Microsemi and the Microsemi logo are registered trademarks or service marks of Microsemi Corporation and/or its affiliates. Third-party trademarks and service marks mentioned herein are the property of their respective owners.
View original content with multimedia:http://www.prnewswire.com/news-releases/microsemi-rtg4-fpgas-become-industrys-first-high-speed-signal-processing-radiation-tolerant-fpgas-to-achieve-qml-class-v-qualification-300699726.html
SOURCE Microchip Technology Inc.
Released August 28, 2018