Daimler Adopts Microchip’s MOST150 Devices With Coaxial Physical Layer for Future Infotainment Network Systems

Microchip’s MOST150 Intelligent Network Interface Controllers With Coaxial Transceiver Significantly Reduce System-Level Cost

CHANDLER, Ariz., Jan. 05, 2017 (GLOBE NEWSWIRE) -- Microchip Technology Inc. (NASDAQ:MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced that Daimler AG plans to utilize Microchip’s OS81118 Intelligent Network Interface Controller (INIC) with integrated coaxial transceiver as its next-generation infotainment networking platform. Daimler expects to significantly reduce costs by moving to coaxial cabling, while retaining all the benefits of their current MOST150-based systems and leveraging their existing designs for fast time to market.

To date, around 200 million Media Oriented Systems Transport (MOST®) interface controllers have been installed in more than 200 car models since 2001. Daimler and most major car makers have successfully implemented MOST technology in their multi-node infotainment networking systems, as it provides a field-proven, low-risk, whole-system solution. The MOST150 standard meets Daimler’s future requirements, and the coaxial physical layer is expected to dramatically reduce Daimler’s costs. This latest version of MOST technology continues to predictably and efficiently transport video, audio, packet and control data throughout the vehicle without time-synchronization protocols, using dedicated channels for minimal processor overhead in the main infotainment control unit.

“The MOST150 coaxial physical layer is helping Daimler develop more cost-competitive infotainment solutions for our demanding customers, and it protects our investments made with MOST technology,” said Reinhold Beck, Senior Manager at Daimler.

“We are grateful for Daimler’s contribution to the specification work on the MOST150 coaxial physical layer as a member of the MOST Cooperation physical layer working group,” said Dan Termer, vice president of Microchip’s Automotive Information Systems Division. “This is a great example of the ongoing and successful cooperation taking place among multiple MOST Cooperation member companies.”

The MOST150 standard also provides 150 Mbps performance and proven electromagnetic-compatibility (EMC) behavior. And, the inherent shielding of its new coaxial-cabling option provides superior EMC immunity.

The MOST Cooperation standards enable automotive OEMs and their Tier 1 suppliers with a proven and well-supported methodology for defining and implementing high-bandwidth infotainment and Advanced Driver Assistance (ADAS) systems, including a standard physical layer and a robust method for system management and control with superior reliability and Quality of Service (QoS). Using MOST technology also results in reduced weight for easier compliance with environmental regulations.

To learn more about Microchip’s MOST® networking products, visit http://www.microchip.com/design-centers/automotive/most/products.

Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):

About Microchip Technology
Microchip Technology Inc. (NASDAQ:MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com.

Note: The Microchip name and logo, the Microchip logo, and MOST are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Tags / Keywords: MOST Cooperation Coaxial Specification, Coaxial Physical Layer, Inherent Shielding Provides Superior EMC Immunity, 150 Mbps INIC With Extended Features, Support for all MOST Data Types, Control, Synchronous, Isochronous, MOST Ethernet Packet Chanel, USB 2.0 High-speed Device (PHY/HSIC), Standard Hardware Interface to SoCs

Editorial Contact:
Sarah Broome
480-792-4386
sarah.broome@microchip.com

Reader Inquiries:
1-888-624-7435

Primary Logo

Source: Microchip Technology Incorporated