Microchip Adds Two New PIC® MCU Families With Core-Independent Peripherals That Enable Functions for a Broad Range of Applications
PIC16F18877 Is the First MCU With ADC Computation and First PIC16 With New Low-Power Modes; PIC16F1579 Is the First 8-bit PIC MCU With 4 Independent Time-Based 16-bit PWMs
CHANDLER, Ariz., July 20, 2015 /PRNewswire/ -- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced from ESC Silicon Valley two new 8-bit families that expand its growing portfolio of innovative PIC® MCUs with Core-Independent Peripherals (CIPs). 8-bit MCUs can now be used in a much broader range of applications, due to the growing number of these intelligent, interconnected CIPs that combine to perform functions autonomously, without the core. Because these functions are deterministically and reliably performed in hardware instead of software, CIPs enable system performance that is far beyond typical 8-bit MCUs while simplifying the design experience and reducing memory cost. Additionally, these two new families are available in 8 to 40-pin packages, reducing board space while serving a wide 1.8 to 5.5V operating range. Both families offer the Peripheral Pin Select feature, which enables flexible pin mapping and PCB routing to minimize EMI and crosstalk. Example applications include consumer electronics, the Internet of Things (IoT), wearable technology and safety-critical systems.
Learn more about the PIC16F1579 Family at http://www.microchip.com/PIC16F1579-072015a, and the PIC16F18877 Family at http://www.microchip.com/PIC16F18877-072015a, and watch short overview videos, here: http://www.microchip.com/Videos-072015a. To view a brief presentation, visit http://www.microchip.com/Presentation-072015a.
The four new members of the PIC16F1579 Family are offered in 14 to 20-pin packages with up to 28 KB of Flash and feature CIPs that enable functions in a broad range of applications, such as LED lighting and motor control. They are the first 8-bit PIC MCUs with four 16-bit PWMs that each have independent timers, for flexible output and signal generation functions, including edge, center-aligned and other output modes. System-communication functions are supported via serial interfaces for LIN and DMX connectivity, while the family's intelligent analog integration enables signal and sensor interface functions.
The first 10 members of the PIC16F18877 Family are available in 8 to 40-pin packages with up to 56 KB of Flash and feature CIPs that enable functions in a broad range of applications, such as consumer electronics, IoT and safety-critical systems. They are the first MCUs to integrate an ADC with computation, which performs input and sensor interface functions such as accumulation, averaging and low-pass filter calculations in hardware instead of software, enabling the CPU to Sleep or execute other tasks. They're also the first PIC16 MCUs to augment Microchip's eXtreme Low Power (XLP) technology with the IDLE and DOZE modes for reduced active power consumption. Additionally, they're the first 8-bit MCUs with Peripheral Module Disable, which completely removes peripherals from the power rail and clock tree for zero power leakage. Other integrated CIPs, such as the Hardware Limit Timer, combine for the easy implementation of safety-critical functions.
"These two new families are the latest examples of Microchip's leadership in the 8-bit MCU market, with the continued expansion of innovative CIPs and intelligent analog that enable functions and capabilities far beyond what traditional 8-bit MCUs could perform," said Steve Drehobl, vice president of Microchip's MCU8 Division. "These families also exemplify Microchip's 'Flexible Intelligence Made Easy' philosophy, as they provide designers with a broad range of intelligent and configurable peripheral options in many low pin count packages and a wide operating voltage range. Development is made easy via our comprehensive platform of software and hardware tools, integrated under our singular MPLAB® X IDE."
Development Support
The Curiosity Development Board (part # DM164137, $20) is available today (http://www.microchip.com/Curiosity-072015a), to enable easy system design. The freely downloadable MPLAB Code Configurator generates code with the click of a button. It provides a visual representation of an MCU's peripherals, eliminating the need to read data sheets. Additionally, it enables the easy setup of CIPs and provides production-ready code, speeding the development efforts of both new and experienced users. Microchip's MPLAB XC8 compiler and standard programmer/debuggers are also available for purchase.
Pricing and Availability
Please click on the following links, to view tables summarizing the availability, and packaging and memory options for the new PIC16F1579 (http://www.microchip.com/PIC16F1579-Table-072015a) and PIC16F18877 (http://www.microchip.com/PIC16F18877-Table-072015a) 8-bit MCU families. Pricing starts at $0.51 each in 10,000-unit quantities. For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at http://www.microchip.com/CIPs-072015a. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip's authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- PIC16F1579 Family Chip Graphic: http://www.microchip.com/PIC16F1579-Graphic-072015a
- PIC16F1579 Family Block Diagram: http://www.microchip.com/PIC16F1579-Diagram-072015a
- PIC16F18877 Family Chip Graphic: http://www.microchip.com/PIC16F18877-Graphic-072015a
- PIC16F18877 Family Block Diagram: http://www.microchip.com/PIC16F18877-Diagram-072015a
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/RSS-072015a
- Twitter: http://www.microchip.com/Twitter-072015a
- Facebook: http://www.microchip.com/Facebook-072015a
- YouTube: http://www.microchip.com/YouTube-072015a
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-072015a.
Note: The Microchip name and logo, PIC, and MPLAB are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: CIP, Function, IoT, Lighting, Power Supplies, 16-bit PWM, LED, RGB, Power Supply, Low Power, Motor Control, Safety Critical
|
Editorial Contact: |
Reader Inquiries: |
|
Eric Lawson |
1-888-624-7435 |
|
480-792-7182 |
|
Logo - https://photos.prnewswire.com/prnh/20141115/158835LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/microchip-adds-two-new-pic-mcu-families-with-core-independent-peripherals-that-enable-functions-for-a-broad-range-of-applications-300115393.html
SOURCE Microchip Technology Inc.
Released July 20, 2015