Microchip Reclaims Top 8-bit Microcontroller Revenue Ranking
2014 Market Share Grows in 8, 16 and 32-bit MCUs; Breaks Into Top 10 for 32-bit
CHANDLER, Ariz., April 27, 2015 /PRNewswire/ -- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, has reclaimed the number-one position in worldwide 8-bit microcontroller (MCU) revenue, according to industry analyst firm Gartner's just-published 2014 rankings. This validates Microchip's unwavering commitment and innovation efforts for its 8-bit PIC® microcontroller portfolio.
While many MCU vendors have deemphasized their 8-bit offerings in recent years, Microchip has continued to innovate across all of its 8-bit, 16-bit and 32-bit product lines. And it continues to grow market share in all three areas, according to Gartner's 2014 report. In the 16-bit MCU market, Microchip was the fastest-growing supplier among the top 10 in 2014, growing at greater than 2X the rate of any of the other top 10 companies. Its 32-bit MCUs broke into the top 10 ranking of 32-bit MCU suppliers for the first time in 2014, based on 42.3% growth.
"We are pleased to report that Microchip has regained the #1 position for 8-bit microcontrollers," said Steve Sanghi, Microchip's president and CEO. "Four years ago, it took the merger of three Japanese semiconductor giants—NEC, Hitachi and Mitsubishi in the form of Renesas—to knock us off the #1 spot for 8-bit MCUs. We said at the time that we would work relentlessly to gain market share and wrest back the #1 spot. Following their merger in 2010, Renesas' 8-bit MCU business was 41% larger than ours. In every year since 2010, we closed the gap, and in 2014 we regained our leadership position, finishing 10.5% higher than Renesas."
8-bit PIC MCUs provide developers with an easy migration path from 6 to 100 pins, with little or no code change required. This MCU portfolio offers product families with varying levels of intelligent integration, including a host of Core Independent Peripherals, which require little to no CPU intervention, freeing the core to perform other application tasks. Also integrated are Intelligent Analog peripherals, including op amps, comparators, ADCs, DACs and CTMUs; Human Interface peripherals for LCD displays and mTouch® capacitive sensing; and Communications channels for Ethernet, I2C™, SPI, USB, CAN and LIN (EUSARTs). The MPLAB® Code Configurator plug-in for Microchip's IDE makes it easy to take advantage of all this integration, by generating seamless, easily understood C code for quick insertion into projects.
Microchip's 8- and 16-bit PIC MCUs combine high performance, low cost, rich analog and digital peripheral integration, and small package size to offer the best price/performance ratio in the industry. PIC MCUs with eXtreme Low Power (XLP) technology provide the industry's lowest power consumption and most advanced low-power features, including Sleep currents down to 9 nA and Active Mode currents down to 30 microamps/MHz, resulting in battery life of up to 20 years or more.
The PIC32 family of 32-bit MCUs is a natural extension to Microchip's portfolio of more than 1,200 PIC microcontroller and dsPIC® digital signal controller (DSC) products. Customers can use Microchip's universal MPLAB X Integrated Development Environment (IDE) to design applications using all of Microchip's 8-, 16-, and 32-bit PIC microcontroller and DSC products, and some of its memory devices. Microchip remains the only company to support all of its standard MCUs and DSCs from a single IDE.
Resources
High-res Photo of CEO Steve Sanghi Available Through Flickr or Editorial Contact (feel free to publish): http://www.microchip.com/Photo-042715a
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/RSS-042715a
- Twitter: http://www.microchip.com/Twitter-042715a
- Facebook: http://www.microchip.com/Facebook-042715a
- YouTube: http://www.microchip.com/YouTube-042715a
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-042715a.
Note: The Microchip name and logo, PIC, dsPIC, MPLAB, and mTouch are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: Microchip, 8-bit, MCU, Market Share, Ranking, 32-bit, 16-bit, Gartner
|
Editorial Contact: |
Reader Inquiries: |
|
Eric Lawson |
1-888-624-7435 |
|
480-792-7182 |
|
Logo - https://photos.prnewswire.com/prnh/20141115/158835LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/microchip-reclaims-top-8-bit-microcontroller-revenue-ranking-300072100.html
SOURCE Microchip Technology Inc.
Released April 27, 2015