Microchip LoRa™ Technology Wireless Module Enables IoT; First Module for Ultra Long-Range and Low-Power Network Standard
Stack-on-Board RN2483 Module Makes it Easy to Tap the 10-Mile Range and 10-Year Battery Life of LoRa Technology Wireless Networks
CHANDLER, Ariz., March 2, 2015 /PRNewswire/ -- [NASDAQ: MCHP] -- Microchip Technology Inc., a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced the first in a series of modules for the LoRa™ technology low-data-rate wireless networking standard, which enables Internet of Things (IoT) and Machine-to-Machine (M2M) wireless communication with a range of more than 10 miles (suburban), a battery life of greater than 10 years, and the ability to connect millions of wireless sensor nodes to LoRa technology gateways. The 433/868 MHz RN2483 is a European R&TTE Directive Assessed Radio Module, accelerating development time while reducing development costs. Additionally, it combines a small module form factor of 17.8x26.3x3 mm with 14 GPIOs, providing the flexibility to connect and control a large number of sensors and actuators while taking up very little space.
To learn more about this new module, go to: http://www.microchip.com/LoRa-Module-030215a. And, visit Microchip at the LoRa Alliance's Mobile World Congress Open House, at 5:30 p.m. on this Wednesday, March 4, at the Miramar Hotel.
"The RN2483 module is a revolutionary end-node IoT solution for the new LoRa technology network, enabling extremely long-range, bidirectional communication with significant battery life," said Steve Caldwell, vice president of Microchip's Wireless Products Division. "As a founding member of the LoRa Alliance, we are working to ensure our modules are compatible with all partner gateways and back-end network service providers."
Gartner predicts that there will be 25 billion connected things in use by 2020. While the IoT market is explosively growing, developers are challenged to establish a simple, robust infrastructure with their limited resources. They are demanding a solution that requires a minimum total cost of ownership and is easy to design, with short time to market, great interoperability and nationwide deployment.
The RN2483 comes with the LoRaWAN™ protocol stack, so it can easily connect with the established and rapidly expanding LoRa Alliance infrastructure—including both privately managed local area networks (LANs) and telecom-operated public networks—to create Low Power Wide Area Networks (LPWANs) with nationwide coverage. This stack integration also enables the module to be used with any microcontroller that has a UART interface, including hundreds of Microchip's PIC® MCUs. Additionally, the RN2483 features Microchip's simple ASCII command interface for easy configuration and control.
LoRa technology has several advantages over other wireless systems. It utilizes a spread-spectrum base modulation that is capable of demodulation with a 20 dB below noise level. This enables high sensitivity with robust network links, improves network efficiency and eliminates interference. The LoRaWAN protocol's star topology eliminates synchronization overhead and hops, compared to mesh networks, which reduces power consumption and enables multiple concurrent applications to run on the network. LoRa technology also has a much longer range than other wireless protocols, which enables the RN2483 to operate without repeaters, reducing the total cost of ownership. In comparison to 3G and 4G cellular networks, LoRa technology is far more scalable and cost effective for embedded applications.
The RN2483 module resolves the age-old wireless developer's dilemma, where they had to choose between longer range and lower power consumption. By employing LoRa technology, designers can now maximize both while reducing the cost of additional repeaters. Additionally, the RN2483 provides them with the ability to secure their network communication using AES-128 encryption.
With its scalability, robust communication, mobility and the ability to operate in harsh outdoor environments, the RN2483 is well suited for a broad range of low-data-rate wireless monitoring and control designs. Example IoT and M2M applications include: Smart Cities (street lights, parking, traffic sensors), Energy Measurement (electricity/water/gas smart meters), and Industrial/Commercial/Home Automation (HVAC controls, smart appliances, security systems, lighting).
Pricing and Availability
Samples of the RN2483 are available now to beta customers, by contacting Microchip's field sales force, and it is expected to be widely available for purchase in May. It will sell for $10.90 each in 1,000-unit quantities. Development boards are also expected to be available for purchase in May, which will allow designers to utilize Microchip's proven and free MPLAB® integrated development environment. For additional information, contact any Microchip sales representative or visit Microchip's Web site at http://www.microchip.com/LoRa-Module-030215a.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Module Photo: http://www.microchip.com/Module-Photo-030215a
- Block Diagram: http://www.microchip.com/Block-Diagram-030215a
Follow Microchip
- RSS Feed for Microchip Product News: http://www.microchip.com/RSS-030215a
- Twitter: http://www.microchip.com/Twitter-030215a
- Facebook: http://www.microchip.com/Facebook-030215a
- YouTube: http://www.microchip.com/YouTube-030215a
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-030215a.
Note: The Microchip name and logo, PIC, and MPLAB are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: LoRa technology, LoRaWAN protocol, LoRa module, RN2483, Long range, long battery life, Low power, end nodes, sensor network, IoT, M2M
|
Editorial Contact: |
Reader Inquiries: |
|
Eric Lawson |
1-888-624-7435 |
|
480-792-7182 |
|
Logo - https://photos.prnewswire.com/prnh/20141115/158835LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/microchip-lora-technology-wireless-module-enables-iot-first-module-for-ultra-long-range-and-low-power-network-standard-300043110.html
SOURCE Microchip Technology Inc.
Released March 2, 2015