Microchip's Free Code Configuration Plug-In for MPLAB® X IDE Makes it Faster and Easier to Develop Firmware on 8- and 16-bit PIC® MCUs

The MPLAB Code Configurator Enables Firmware Developers to Quickly Initialize the Device and Implement Peripheral Drivers for Faster Time to Market

CHANDLER, Ariz., Jan. 26, 2015 /PRNewswire/ -- [NASDAQ:  MCHP] — Microchip Technology Inc., a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced  the expansion of its MPLAB® Code Configurator Plug-In to support 16-bit PIC® MCUs, in addition to the 8-bit devices already supported.  This code development tool enables developers to enhance the design experience with faster application development.  Based on the popularity of this tool for 8-bit products, Microchip has added support for more than 50 16-bit devices into the latest release of the MPLAB Code Configurator.

Microchip Technology Inc. is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com.

To learn more about Microchip's MPLAB® Code Configurator Plug-In, visit:  http://www.microchip.com/MPLABCodeConfig-Page-012615a

The MPLAB Code Configurator is a free user friendly plug-in tool for the MPLAB® X Integrated Development Environment (IDE) that leverages drivers and GUI for controlling and driving the peripherals inside PIC microcontrollers with simple and clearly documented driver APIs.  The configurator tool simplifies software development, using an intuitive GUI to configure peripherals, accelerating time to market for customers designing with 8- and 16-bit PIC microcontrollers.  It is easy to change peripheral configurations or add/remove peripherals from your project.  Also, the generated code is reliable and designed for efficient use of CPU and memory resources. 

The tool offers many powerful features such as visual setup for I/O pin management with both a chip-level and tabular view.  Also, once a system-level clock rate is set, the tool will automatically calculate timer periods, duty cycles and baud rates for peripherals.  With a simple drag-and-drop style interface, this tool generates easy-to-read code that includes peripheral configuration setup, drivers and pin mapping to efficiently solve application development obstacles.  Designers can benefit from this easy-to-use code development solution, which is better able to meet their ever-shorter product design schedules and decreasing budgets.  

 "The MPLAB Code Configurator not only simplifies the development effort, but also reduces time to market," said Joe Thomsen, vice president of Microchip's MCU16 Division.  "This tool, which now includes support for PIC24 families, provides a simple graphical interface to setup the device peripherals and pins, giving users a head start in their application code development."

The MPLAB Code Configurator is available today, via a free download from http://www.microchip.com/MPLABCodeConfig-Page-012615a.  More than 50 16-bit PIC MCU products in six different families are now supported in this latest release, including the PIC24FJ128GA310, PIC24F16KM204, PIC24FJ128GC010, PIC24FJ128GB204, PIC24FJ64GB004 and PIC24FJ64GA104 families.  In addition, more than 140 8-bit PIC MCU products are supported in the latest release including the newly added PIC16LF155X, PIC16F161X, PIC16F17XX and PIC18F14K22 families.

Resources
High-res Photo Available Through Flickr or Editorial Contact (feel free to publish):

Follow Microchip:

About Microchip Technology
Microchip Technology Inc. (NASDAQ:  MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide.  Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality.  For more information, visit the Microchip website at http://www.microchip.com/Homepage-012615a.

Note:  The Microchip name and logo, MPLAB, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries.  All other trademarks mentioned herein are the property of their respective companies.

Tags / Keywords:  MPLAB, Code Configurator, Development Tool, Plug-In, MCC

 

Editorial Contact:

Reader Inquiries:

Terri Thorson

1-888-624-7435

480-792-4386

http://www.microchip.com/MPLABCodeConfig-Page-012615a

terri.thorson@microchip.com


 

Logo - https://photos.prnewswire.com/prnh/20141115/158835LOGO

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/microchips-free-code-configuration-plug-in-for-mplab-x-ide-makes-it-faster-and-easier-to-develop-firmware-on-8--and-16-bit-pic-mcus-300024572.html

SOURCE Microchip Technology Inc.