Microchip Releases Fourth Generation JukeBlox® Wi-Fi® Platform for the Ultimate Streaming Audio Entertainment Experience

Wireless Module and SDK Deliver New Features for Developing High Quality Audio Products at Competitive Consumer Price Points

CHANDLER, Ariz., Dec. 8, 2014 /PRNewswire/ -- [NASDAQ:  MCHP] -- Microchip Technology Inc., a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced the release of its fourth generation JukeBlox® platform that enables audio brands to develop high quality, low-latency products such as standalone or multi-room wireless speakers, AV receivers, mini and micro systems, and sound bars. Microchip's new JukeBlox 4 Software Development Kit (SDK) in combination with its CY920 Wi-Fi® & Bluetooth® Network Media Module includes next-generation dual-band Wi-Fi technology, MultiZone/multi-room features, AirPlay® and DLNA® connectivity as well as integrated music services to enhance the consumer's listening experience. Additional cost-saving features lower bill of materials and enable competitively priced consumer products.

Microchip Technology Inc. is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com.

The certified CY920 Wi-Fi and Bluetooth Network Media Module is based on Microchip's new, low-cost DM920 Wi-Fi Network Media Processor, which integrates 2.4 GHz and 5 GHz 802.11a/b/g/n Wi-Fi, high-speed USB 2.0 and Ethernet connectivity. Speakers utilizing the 5 GHz band avoid the RF congestion found in the 2.4GHz band, resulting in fewer audio drops and the ability to use a greater number of speakers in multi-room/whole-home audio systems.

The DM920 Wi-Fi Network Media Processor also features integrated dual 300 MHz DSP cores that can reduce or eliminate the need for costly standalone DSP chips. An easy-to-use, PC-based graphical user interface (GUI) simplifies the use of a pre-developed suite of standard speaker-tuning DSP algorithms, including a 15-band equalizer, multiband dynamic range compression, equalizer presets and various filter types. Engineers with no DSP code-writing experience can easily implement DSP into their designs, while experienced DSP engineers can harness the full power of an industry-standard DSP architecture.

With JukeBlox 4, product developers can build solutions equipped to directly stream cloud-based music services such as Spotify® Connect, Qobuz, Rhapsody, Deezer and many others while using mobile devices as remote controls. This allows mobile devices to move anywhere in the Wi-Fi network without interrupting music playback, and it greatly increases battery life. JukeBlox technology continues to offer seamless cross-platform support for iOS, Android™, Windows® 8 and Mac®, along with a complete range of audio codecs and ease-of-use features to simplify network setup.

Additionally, the SDK has whole-home audio (MultiZone/multi-room) functionality for simultaneous audio streaming to, and control of, multiple JukeBlox platform-enabled devices in the home. The combination of new hardware and software technology improves synchronization and reduces network bandwidth utilization to achieve a robust audio streaming experience.

"With over eight million modules shipped to date, the JukeBlox platform was an early pioneer in the streaming-audio market and has been adopted by more audio brands than any other platform available for Wi-Fi audio connectivity," said Sumit Mitra, vice president of Microchip's Wireless Solutions Group. "Building on our unequaled position in the wireless audio market, the fourth generation JukeBlox SDK and CY920 network module are in production now with lead customers."

Availability
The JukeBlox 4 SDK, paired with the JukeBlox CY920 module, is available today for sampling and volume production. For additional information, contact any Microchip sales representative, or visit Microchip's Web site at http://www.microchip.com/JukeBlox-Page-120814a.

Resources:
High-res Images Available through Flickr or Editorial Contact (feel free to publish):

Follow Microchip:

About Microchip Technology
Microchip Technology Inc. (NASDAQ:  MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-120814a.

Note:  The Microchip name and logo, and JukeBlox are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Tags / Keywords:  JukeBlox, MultiZone, AirPlay, Spotify Connect, Qobuz, music streaming, networked audio processor, CY920, DM920, wireless audio, whole home audio

Editorial Contact:

Reader Inquiries:

Eric Lawson

1-888-624-7435

480-792-7182

http://www.microchip.com/JukeBlox-Page-120814a

eric.lawson@microchip.com


Logo - https://photos.prnewswire.com/prnh/20141115/158835LOGO

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/microchip-releases-fourth-generation-jukeblox-wi-fi-platform-for-the-ultimate-streaming-audio-entertainment-experience-300006148.html

SOURCE Microchip Technology Inc.