New High-Speed A/D Converters from Microchip Feature Industry’s Lowest-Power 16-bit, 200 Msps Stand-Alone ADCs
MCP37DX1-200 and MCP372X1-200 Families Provide Low Power and High Integration of Digital Processing Functions in 124-lead VTLA Packages
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ:MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced two families of new high-speed A/D converters in the MCP37DX1-200 and MCP372X1-200 families. These families feature 12-, 14- and 16-bit pipelined A/D converters with a maximum sampling rate of 200 Mega samples per second (Msps). The 14- and 16-bit devices feature high accuracy of over 74 dB Signal-to-Noise Ratio (SNR) and over 90 dB Spurious Free Dynamic Range (SFDR), while the 12-bit devices have 71.3 dB SNR and 90 dB SFDR. This enables high-precision measurements of fast input signals. These families operate at very low-power consumption of 490 mW at 200 Msps including LVDS digital I/O. Lower power-saving modes are available at 80 mW for standby and 33 mW for shutdown.
The MCP37DX1-200 and MCP372X1-200 include various digital processing features that simplify system design, cost and power usage for designers. These families also include decimation filters for improved SNR, individual phase, offset and gain adjustment and a fractional delay recovery for time-delay corrections in multi-channel modes. Data is available through the serial DDR LVDS or parallel CMOS interface and configured via SPI. An integrated digital down-converter is included in the MCP37DX1-200 family making it ideal for communications applications. The 12-bit families include an integrated noise-shaping requantizer, which enables users to lower the noise within a given band of interest for improved accuracy and performance. These families are targeted for applications in the communications markets such as base stations, test equipment, and IF receivers, among others.
“Microchip has entered the market of high-performance, high-speed A/D converters while leaping past existing solutions with industry-leading low-power performance,” said Bryan J. Liddiard, marketing vice president of Microchip’s Analog and Interface Products Division. “With their low power and high integration of digital processing functions, these new A/D converters are ideal for many communication systems, industrial and other applications.”
Development Tool Support
The MCP37DX1-200 and MCP372X1-200 are supported by Microchip’s MCP37XXX-200 16-bit VTLA Evaluation Board (Part # ADM00505, $399.00), Microchip’s MCP37XXX-200 12-bit VTLA Evaluation Board (Part # ADM00619, $399.00) and MCP37XXX-200 Data Capture Card (Part # ADM00506, $599.00).
Pricing & Availability
The MCP37DX1-200 and MCP372X1-200 families are available now for sampling and volume production in 124-lead VTLA packages, at prices ranging from $29.58 to $96.07 each, in 5,000-unit quantities.
For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/MCP37DX1-200_MCP372X1-200-Page--111214a. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Chip Graphic: http://www.microchip.com/Chip-Graphic-111214a
- Block Diagram: http://www.microchip.com/Block-Diagram-111214a
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/RSS-111214a
- Twitter: http://www.microchip.com/Twitter-111214a
- Facebook: http://www.microchip.com/Facebook-111214a
- YouTube: http://www.microchip.com/YouTube-111214a
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/Homepage-111214a.
Note: The Microchip name and logo is a registered trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: ADC, A/D Converter, High Speed, Low Power, Communications Systems, Data Converter, Digital-Down Converter, Decimation Filter, MCP37DX1-200, MCP372X1-200, MCP37D31-200, MCP37231-200, MCP37D21-200, MCP37221-200, MCP37D11-200, MCP37211-200
Microchip Technology Inc.
Editorial Contact:
Terri
Thorson, 480-792-4386
terri.thorson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/MCP37DX1-200_MCP372X1-200-Page--111214a
Source: Microchip Technology Inc.
Released November 12, 2014