Microchip’s New 2.4 GHz RF High-Power Amplifier Offers Low EVM and Current for 256-QAM and 802.11b/g/n; Extends Range of Ultra-High Data Rate WLANs
SST12CP21 Combines High Linear Output Power With Low Current in Small Package for Longer Range and High Data Rate WLANs
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced its latest 2.4 GHz 256-QAM RF high-power amplifier—the SST12CP21—which offers ultra low EVM and current consumption for 256-QAM and IEEE 802.11n systems. The SST12CP21 delivers high linear output power of up to 23 dBm at 1.75% dynamic EVM, with MCS9 HT40 MHz bandwidth modulation at 5V and 320 mA current consumption. Additionally, the SST12CP21 delivers 25 dBm linear power at 3% EVM with only 350 mA current consumption for 802.11g/n applications. This performance significantly extends the range of 802.11b/g/n WLAN and MIMO systems, while consuming extremely low current at the maximum 256-QAM data rate. The SST12CP21 is also spectrum mask compliant up to 28 dBm for 802.11b/g communication. Board space is reduced by the small 3x3x0.55 mm, 16-pin QFN package that matches a popular pin-out.
Achieving the maximum data rate and longest range while minimizing current consumption is essential to Wi-Fi® MIMO access-point, router and set-top-box system designers. The SST12CP21 power amplifier has a low operating current of 320 mA at 23 dBm and 350 mA at 25 dBm, which enables multichannel and higher data rate WLAN systems. This amplifier also features 50 ohm on-chip input match and simple output match, which is easy to use and reduces board size. Additionally, the integrated linear power detector provides accurate output power control over temperature and 2-to-1 output mismatch.
“Microchip’s RF power amplifiers have a strong position in the WLAN market, due to their reliability combined with high-power efficiencies that can only be achieved using InGaP/GaAs HBT,” said Daniel Chow, vice president of Microchip’s RF Division. “The SST12CP21 provides the same reliable operation over temperature, at an even lower EVM. In conjunction with its higher-efficiency operation of only 320 mA at 23 dBm at 1.75% EVM, and 350 mA at 25 dBm at 3% EVM, this new power amplifier extends the range of both 802.11n and ultra-high data rate, 256-QAM MIMO systems.”
Development Support
Evaluation boards for the new SST12CP21 power amplifiers are available through Microchip’s sales representatives.
Pricing & Availability
The SST12CP21 is available today for sampling and volume production, in the popular 3x3x0.55 mm, 16-pin QFN package. Pricing is $0.754 each, in 10,000-unit quantities.
For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s website at http://www.microchip.com/get/L3PX. To purchase products mentioned in this press release, go to microchipDIRECT (http://www.microchip.com/get/VQCH) or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Chip Graphic: http://www.microchip.com/get/3DHN
- Block Diagram: http://www.microchip.com/get/U4MN
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/M4K7
- Twitter: http://www.microchip.com/get/BQWR
- Facebook: http://www.microchip.com/get/AAVU
- YouTube: http://www.microchip.com/get/B1XM
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/6VCH.
Note: The Microchip name and logo is a registered trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: 2.4 GHz, High Power Amplifier, 256 QAM Modulation
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/L3PX
Source: Microchip Technology Inc.
Released August 25, 2014