Microchip Unveils 4Kb Serial Presence Detect EEPROM for DDR4 SDRAM Modules
SPD EEPROM Device Designed to Meet New DDR4 Standard for PCs and Laptops
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today introduced a new 4Kb I2C™ Serial Presence Detect (SPD) EEPROM device—the 34AA04. This device is specifically designed to work with the next generation of Double Data Rate 4 (DDR4) SDRAM modules used in high-speed PCs and laptops, while also supporting older DDR2/3 platforms.
This new device is designed for the price-competitive consumer products market and is capable of operation across a broad voltage range (1.7V to 3.6V). This device is JEDEC JC42.4 (EE1004-v) Serial Presence Detect (SPD) compliant and is designed to be compatible with DDR4 SDRAM modules. The 34AA04 includes reversible software write protection for each of four independent 128 x 8-bit blocks and supports a new SMBus compatible bus time out. The device features a page write capability of up to 16 bytes of data and 3 address pins allow up to eight devices on the same bus.
The 34AA04 is backward compatible with existing DDR2 and DDR3 SPD EEPROMs. To ensure backward compatibility, the memory array of the 34AA04 is divided into two separate 256-byte banks to overlay with the architecture of older SPD EEPROM devices. The 34AA04 serves a wide range of applications in the consumer-electronic market (e.g., PCs, laptops, graphic cards), among others.
“Microchip has supported the DRAM market with SPD EEPROMs in prior DDR1, DDR2 and DDR3 platforms and is pleased to announce our new JEDEC-Compliant SPD EEPROM devices for the DDR4 DIMM modules,” said Randy Drwinga, vice president of Microchip’s Memory Products Division. “The reversible software write-protect on four individual blocks, faster data rates and SMBus compatibility offers DRAM manufacturers added flexibility to enable new features in the high-speed PC, laptop and graphic card markets.”
Pricing & Availability
The 34AA04 devices are available today for sampling and volume production, in 8-pin SOIC, TDFN, UDFN, TSSOP and PDIP packages, starting at $0.20 each, in 10,000 unit quantities.
For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/CKQL. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Chip Graphic: http://www.microchip.com/get/E2SE
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/XTAQ
- Twitter: http://www.microchip.com/get/EE5C
- Facebook: http://www.microchip.com/get/960K
- YouTube: http://www.microchip.com/get/X0A5
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal analog, and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/KQMK.
Note: The Microchip name and logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: SPD EEPROM, DDR4, DIMM, DDR4 SDRAM, Serial Presence Detect, JEDEC, DDR4 EEPROM, DDR
Microchip Technology Inc.
Editorial Contact:
Terri
Thorson, 480-792-4386
terri.thorson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/CKQL
Source: Microchip Technology Inc.
Released April 14, 2014