Microchip’s Low-Power Sensor Hub Makes Sensor Fusion Easy; Partnered With Leading Sensor Manufacturers for Maximum Flexibility
Windows® 8-based PCs, 2-in-1 Convertibles, Tablets and Gaming Applications Can Easily Access Motion and Position Data via Turnkey Solution
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced the SSC7102—a low-power, flexible and turnkey sensor hub that makes implementing sensor fusion easy and provides an extremely large selection of supported sensors. In fact, Microchip directly partnered with multiple industry-leading sensor manufacturers and sensor-fusion specialists to create this solution, enabling faster time to market without the need for sensor-fusion expertise. The SSC7102 is also extremely efficient. It consumes ~4 mA while running complex sensor-fusion algorithms, resulting in longer battery life for Windows® 8.1 tablets, laptops, ultrabooks and smart phones.
Sensors can now be added to virtually anything, due to their small cost and size. IHS iSuppli predicts that more than 6 billion motion sensors are expected to ship in mobile handsets and tablets by 2016. As sensors continue to surround us, system requirements are moving from simple monitoring to providing complex information about our environment and activities. Data from multiple sensors, such as motion (accelerometers, magnetometers, gyroscopes) and environmental (light, temperature, humidity, pressure), needs to be incorporated or “fused” in the system. Microchip’s low-power SSC7102 sensor hub runs these complex sensor-fusion algorithms, while providing maximum flexibility in an easy-to-implement solution.
“Microchip has long been a leader in embedded controllers for PCs and laptops,” said Patrick Johnson, vice president of Microchip’s Computing Products Group. “As the PC platform evolves with ultrabooks and tablets, Microchip is extending its portfolio to support the growing need for motion data. In developing the SSC7102, we partnered with industry-leading companies such as Bosch and Movea to deliver an easy-to-use, Windows 8.1-certified HID-over-I2C™ solution with exceptionally low power consumption.”
Pricing & Availability
Microchip’s SSC7102 sensor hub is available in a 6mm x 6mm body, BGA package, and is priced at $2.69 each in 10,000-unit quantities. Samples are available now, via Microchip’s sales representatives, and volume production is expected by the end of this quarter. For more information, visit http://www.microchip.com/get/9821.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Chip Graphic: http://www.microchip.com/get/T6MB
- System Diagram: http://www.microchip.com/get/A9GQ
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/DN2L
- Twitter: http://www.microchip.com/get/0874
- Facebook: http://www.microchip.com/get/38PP
- YouTube: http://www.microchip.com/get/1WVD
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/VJUG.
Note: The Microchip name and logo is a registered trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: Sensor Hub, Sensor Fusion, MEMS, Windows, Bosch, Movea, Invensense, Accelerometer, Magnetometer, Gyro, Embedded, Mobile, Tablet, Smartphone, Ultrabook, Medical, SMSC
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/9821
Source: Microchip Technology Inc.
Released January 6, 2014