Microchip’s New 2.4 GHz 50 ohm Matched RF Front End Module for 256-QAM, Wi-Fi® and Bluetooth® Extends Mobile Device and Router Ranges
High Linearity and Gain SST12LF09 Integrates Tx Power Amplifier, Rx Low-Noise Amplifier and Low-Loss Single-Pole 3-Throw Antenna Switch Into Small Package
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced its latest 2.4 GHz, 50 ohm Matched RF WLAN Front End Module (FEM)—the SST12LF09—for Bluetooth® connectivity, as well as 802.11b/g/n and 256-QAM Wi-Fi® applications. The SST12LF09 integrates a transmitter power amplifier, a receiver low-noise amplifier, and a low-loss, single-pole three-throw antenna switch for Bluetooth connectivity into one compact 2.5x2.5x0.4 mm, 16-pin QFN package, making it ideal for high-data-rate wireless applications. With its high linear output power of up to 15 and 17 dBm for 1.8% dynamic EVM at 3.3V and 5V, respectively—along with 17 and 18.5 dBm linear power for 3% EVM at 3.3V and 5V, respectively—this FEM significantly extends the range of IEEE 802.11b/g/n WLAN systems while providing excellent transmit power at the maximum 256-QAM data rate. The receiver has a 12 dB gain and a greater than -6 dBm input (1 dB) compression level. In the LNA bypass mode, the receiver has a 9 dB loss and an 8 dBm input compression level.
Attaining the maximum data rate, longest range and highest integration in a small package is essential to the designers of mobile devices, multi-channel access point/routers and set-top boxes. Developers can take advantage of the SST12LF09’s small package size and extra output power at 5V bias to reduce the board size and complexity of their designs while boosting their products’ output power. This FEM also features 50 ohm on-chip input and output match, which is easy to use and shortens time to market.
“Microchip’s 2.4 GHz 256-QAM power amplifiers are generating a high level of interest within the WLAN market, due to their high linear power and efficiency,” said Daniel Chow, vice president of Microchip’s RF Division. “With the release of the SST12LF09, Microchip is building on that reputation with a compact, 256-QAM front end module that offers the same reliable, high-efficiency operation and low dynamic EVM over temperature, while adding a low-noise receiver, which combine to extend the range of 2.4 GHz ultra high data rate mobile devices, routers and set-top boxes.”
Development Support
Evaluation boards for the new SST12LF09 front-end module are available through Microchip’s sales representatives.
Pricing & Availability
The SST12LF09 is available today for sampling and volume production, in a 2.5x2.5x0.4 mm, 16-pin QFN package. Pricing is $0.60 each, in 10,000-unit quantities.
For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/95TE. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Chip Graphic: http://www.microchip.com/get/GDNX
- Block Diagram: http://www.microchip.com/get/E1NT
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/F0UQ
- Twitter: http://www.microchip.com/get/DU98
- Facebook: http://www.microchip.com/get/Q61X
- YouTube: http://www.microchip.com/get/NXWL
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/EN1L.
Note: The Microchip name and logo is a registered trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: 2.4 GHz, Front End Module, 256 QAM Modulation
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/95TE
Source: Microchip Technology Inc.
Released November 21, 2013