Microchip’s BodyCom™ Technology Is World’s First to Use Human Body as a Secure, Low-Power Communication Channel
Framework Provides Short-Range, Low-Data-Rate Communication Solution for Securely Connecting to Wide Range of Wireless Applications
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced from the Embedded World conference in Germany its BodyCom™ technology, which provides designers with the world’s first framework for using the human body as a secure communication channel. Compared to existing wireless methods, BodyCom technology provides lower energy consumption, while further increasing security via bidirectional authentication. Because no RF antennas are required, BodyCom technology allows for simpler circuit-level designs and a lower bill of materials (BOM). All of this is enabled by the BodyCom Development V1.0 Framework, which is supplied through free software libraries that work on all of Microchip’s more than 900 8-, 16- and 32-bit PIC® microcontrollers.
Watch a short video on BodyCom(TM) technology: http://www.microchip.com/get/9TMM
Watch a short video: http://www.microchip.com/get/9TMM
View a brief presentation: http://www.microchip.com/get/G3E2
BodyCom technology is activated by capacitively coupling to the human body. The system then begins communicating bidirectionally between a centralized controller and one or more wireless units. There are a broad range of applications where secure wireless communication is essential, and there is no more secure channel than the human body. This is especially true when you add bidirectional authentication that supports advanced encryption, such as KeeLoq® technology and AES. For example, BodyCom technology helps prevent the “Relay Attack” problem that is typical in automotive passive-keyless-entry security systems.
Most secure, short-range communication designs are battery powered and highly cost constrained. BodyCom technology significantly increases battery life by eliminating the need for a wireless transceiver or high-power inductive fields. It also simplifies development and lowers BOM costs by not only making antenna design unnecessary, but also by using a low-frequency framework with a common microcontroller and standard AFE frequencies (125 kHz and 8 MHz)—no external crystals are needed. And, because it complies with FCC Part 15-B for radiated emissions, BodyCom technology eliminates the cost and complexity of certification.
Additional example applications include Access Control (security systems, home/industrial door locks, pet doors); Personal Safety & Security (equipment access/disable, power tools, firearms, computer systems); Medical (patient monitoring, hospital-room access, equipment tracking); and Consumer (profile management for gaming consoles and exercise equipment).
“BodyCom technology provides a more secure, low-cost and easy method for implementing short-range, low-data-rate wireless communication with the lowest power consumption,” said Steve Drehobl, vice president of Microchip’s MCU8 Division. “Our BodyCom Development Framework is available via free download, and it works with any of our PIC microcontrollers, which presents a very low barrier of entry for designers.”
Development Support
To further enable development and speed time to market, Microchip is also announcing the BodyCom Development Kit (part # DM160213). This kit is available today for $149, and comes with a central controller unit and two wireless mobile units.
The free BodyCom Development V1.0 Framework is also available today, and comes with a communication library, application code examples and a development GUI for use on personal computers. Additionally, application note AN1391, which provides an introduction to BodyCom technology, is available at http://www.microchip.com/get/GA5E.
For more information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/GA5E. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- Photo: http://www.microchip.com/get/9TP0
- Block Diagram: http://www.microchip.com/get/59BR
- Tool: http://www.microchip.com/get/VX2M
Video Available Through YouTube or Editorial Contact (feel free to post): http://www.microchip.com/get/9TMM
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/P2EQ
- Twitter: http://www.microchip.com/get/445D
- Facebook: http://www.microchip.com/get/965T
- YouTube: http://www.microchip.com/get/KUEL
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/DF06.
Note: The Microchip name and logo, PIC, and KeeLoq are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. BodyCom is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: BodyCom, Embedded Security, Passive Keyless Entry, Secure Communications, Secure Access Control, Authentication
Photos/Multimedia Gallery Available: http://www.businesswire.com/multimedia/home/20130226005488/en/
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/GA5E
Source: Microchip Technology Inc.
Released February 26, 2013