High-Current, High-Voltage and High-Performance Applications Benefit From Microchip’s New LDO Voltage-Regulator Family

LDOs Provide High Output Current of 300 mA, High Input Voltage of 16V and High Noise Rejection of 70 dB With Industry’s Best Combination of Performance, Size and Price

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced the MCP1755 and MCP1755S high-performance, high-input-voltage and high-output-current family of CMOS Low-Dropout (LDO) voltage regulators. These LDOs can accept a wide input voltage range of 3.6-16V and deliver an output current of 300 mA at output voltages of 1.8-5.5V, while consuming only 68 µA of quiescent current (typical). Additionally, the MCP1755/1755S LDOs have a shutdown pin, enabling them to consume less than 0.1 µA (typical) during shutdown mode, which extends battery lifetimes. To conserve space, the LDOs are offered in SOT and 2x3 mm DFN packages. These features provide designers with a high degree of flexibility for an extremely broad range of applications, such as medical, mobile devices and LED lighting controllers.

Many of today’s electronic designs need to operate in environments that contain high levels of electrical and magnetic noise. Noise is generated when switching transients and RF signals get coupled onto power-supply lines. Applications such as GFCI and AFCI circuit breakers, wireless devices, automotive-aftermarket electronics, and medical devices are sensitive to this power-supply noise. The MCP1755 and MCP1755S LDOs have a high Power Supply Rejection Ratio (PSRR) of 70 dB @ 1 kHz, which filters input noise and provides significantly cleaner output voltages, making them well suited for noise-sensitive applications.

“The MCP1755/S LDOs are ideal for designs with 9V and 12V power-supply rails, and their higher output current expands our high-performance LDO portfolio into a broader range of applications,” said Bryan J. Liddiard, marketing vice president of Microchip’s Analog & Interface Products Division. “Additionally, the high PSRR of these voltage regulators is great for applications that require very clean supply voltages.”

Pricing and Availability

Both of the new LDOs are available today for sampling and volume production, starting at $0.45 each in 5,000-unit quantities. The MCP1755S is offered in 3-pin SOT223 and 8-pin, 2x3 mm DFN packages. The MCP1755 is available in 5-pin SOT223 and SOT23 packages, as well as the 8-pin, 2x3 mm DFN. For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/LMUT. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.

Resources

High-res Photo & Circuit Diagram Available Through Flickr or Editorial Contact (feel free to publish):

Follow Microchip:

About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/TGB3.

Note: The Microchip name and logo is a registered trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Tags / Keywords: Microchip, MCHP, LDO, Voltage Regulator, PSRR, Shutdown, High Input Voltage, High PSRR, High Output Current

Microchip Technology Inc.
Editorial Contact:
Eric Lawson, 480-792-7182
eric.lawson@microchip.com
Reader Inquiries:
1-888-624-7435
http://www.microchip.com/get/LMUT

Source: Microchip Technology Inc.