Microchip and Digilent® Add Arduino™ Compatible chipKIT™ uC32™ Development Platform and Wi-Fi® Shield for 32-bit PIC® Microcontrollers

New Tools Available from Newark at Special Engineering-Week Discount; Enable chipKIT and Arduino User Communities to Easily Develop Wireless Applications

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, and Digilent®, Inc., today announced the jointly developed chipKIT™ uC32™ open-source development platform, which is based on Microchip’s 32-bit PIC32 microcontroller, as well as the chipKIT Wi-Fi® Shield. Digilent’s chipKIT uC32 development board has the same form factor as their chipKIT Uno32™ board, with the addition of larger memory (512 KB Flash and up to 32 KB RAM). The uC32 board provides a single, general-purpose development platform for users to create a wide range of 32-bit MCU-based applications using the free, Arduino™ compatible chipKIT IDE—called the Multi-Platform IDE, or “MPIDE.” Digilent’s chipKIT Wi-Fi Shield enables users to implement wireless projects with the chipKIT line of microcontroller boards, such as the new uC32, or existing Uno32 and Max32™ boards.

In honor of National Engineer’s Week, Newark is offering the uC32 in a discounted bundle with the chipKIT Basic I/O Shield and PICkit™ 3 In-Circuit Debugger for $84.85—a 30% savings. This “chipKIT Educational Starter Pack” bundle is available now through March 16 at http://www.microchip.com/get/CQGG.

Introduced in May 2011, the PIC32 MCU-based chipKIT Platforms have enabled hobbyists and academics to easily and inexpensively add electronics to their projects, even if they don’t have an engineering background. The chipKIT uC32 board includes Microchip’s PIC32MX340F512H microcontroller, featuring 105 DMIPS performance, 512 KB Flash, 32 KB SRAM and 42 I/O pins that support a number of peripheral functions, such as UART, SPI and I2C™ ports and pulse-width-modulated outputs. Twelve of the PIC32’s I/O pins can be used as analog inputs or as digital inputs and outputs.

Digilent’s chipKIT Wi-Fi Shield makes use of Microchip’s agency-certified MRF24WB0MA Wi-Fi module, and provides chipKIT microcontroller boards with the ability to communicate via IEEE 802.11 compatible wireless networks. The Wi-Fi Shield also provides a microSD™ card connector for use with microSD Flash memory cards. The chipKIT MPIDE SD library can be used to read/write files stored on the microSD card.

“We’re very impressed with the quality and utility of the latest chipKIT development boards from Digilent, and with the robust application libraries they provide for the user community,” said Derek Carlson, Microchip’s vice president of Development Tools.

“The growing popularity of our chipKIT line drives us to create more state-of-the-art products for people, with or without electronic-engineering backgrounds, to easily integrate electronics into their projects,” said Clint Cole, president of Digilent, Inc. “The addition of our chipKIT uC32 and Wi-Fi Shield lets users build a wide range of embedded-system projects with Wi-Fi functionality.”

The MPIDE also makes it easy for new developers to introduce their own compatible chipKIT boards. The MPIDE includes libraries, such as Brian Schmalz’s SoftPWMServo library, which enables users to generate an analogWrite-style output, as well as an RC Servo output, on all pins simultaneously.

Pricing & Availability

The chipKIT uC32 (part # TDGL017) is priced at $34.99 each, and the chipKIT Wi-Fi Shield (part # TDGL016) at $49.99 each. Both boards can be purchased today, at microchipDIRECT or Digilent’s e-Commerce site. For more information, please visit the Digilent Web site at http://www.microchip.com/get/T23G, or contact Alex Wong at awong@digilentinc.com or (509) 334-6306. More information is also available on Microchip’s Web site, at http://www.microchip.com/get/9AAD, as well as the online chipKIT forum and Wiki.

Resources

High-res photos available through editorial contact or Flickr (feel free to publish):

Video (feel free to embed on your site): http://www.microchip.com/get/922J

Follow Microchip:

About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site at http://www.microchip.com/get/SJ4S.

Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. chipKIT, and PICkit are trademarks of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, Arduino, development tool, open source, electronic hobbyist, electronics, wifi shield

Microchip Technology Inc.
Editorial Contact:
Eric Lawson, 480-792-7182
eric.lawson@microchip.com
Reader Inquiries:
1-888-624-7435
http://www.microchip.com/get/T23G

Source: Microchip Technology Inc.