Microchip Launches World’s First Wireless Audio Platform for iOS, Android™, Windows® 8 and Mac®—the New JukeBlox® 3.2 SDK
Latest Software Development Kit Also Adds Seamless Integration of Cloud-Based Music Services and Simultaneous Wi-Fi® Audio Streaming to Multiple Home Audio Products
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, today announced the first and only Wi-Fi® audio connectivity platform—featuring the new JukeBlox® 3.2 platform and software development kit—to support all of the major mobile and PC operating systems along with the DLNA® standard. This includes seamless support for iOS/AirPlay®, Android™, Windows® 8 (mobile and PC), and Mac® in one solution. JukeBlox 3.2 operates on all of Microchip’s existing JukeBlox network media processors and modules, and further adds JB Cloud, which enables a compelling new consumer experience by directly streaming cloud-based music services while using mobile devices as remote controls. This eliminates the need for mobile devices to act as servers, where they consume power and must stop the music to take phone calls or support other personal audio functions, freeing them up to be what they were intended to be—personal communication and Internet devices. Additionally, the SDK has expanded whole-home audio functionality via JB MultiZone 2.0, enabling more robust and extensive simultaneous synchronized audio streaming and control to multiple JB-enabled devices in the home.
Because Microchip’s JukeBlox Platform is the first wireless audio connectivity platform to provide compatibility with all of the major operating systems and audio-interoperability standards in a comprehensive SDK, it is the best and only complete solution for developers. This platform includes SoCs and modules for Wi-Fi networking and media processing, an application software layer for mobile devices and control interfaces, peripheral interfaces and control, and GUI options. And, it is cost effective enough to enable consumer products that retail for as low as $129.
The new JB Cloud software offers product developers and Internet music service providers a compelling new use case and architecture for enabling direct cloud music service streaming with mobile device control—all managed from the native music service app. This dramatically improves the consumer’s in-home experience, enables many more product companies to provide support for the music services, and significantly reduces the support and maintenance for both product companies and service providers, as user control is managed from the service provider’s native app.
The JukeBlox Platform’s expanded MultiZone 2.0 capability supports all the core technologies needed for compelling whole-home audio applications, including the discovery, pairing, group management, control, streaming and synchronization of any audio input source to multiple JB-enabled devices throughout the home. This high-value feature enables the next generation of interoperability between devices, and potentially across brands, helping consumers realize the full potential of their networked audio products.
“Networked audio is the future of home electronics, and JukeBlox 3.2 is enabling that future, today,” said Gene Sheridan, senior vice president and general manager of SMSC, a wholly owned subsidiary of Microchip Technology Inc. “For the first time ever, one wireless audio platform is compatible with iOS, Android and Windows, while enabling a whole-home audio experience with seamless integration of cloud-based music services.”
Pricing & Availability
The JukeBlox 3.2 SDK, paired with any JukeBlox network media processor or module, is available today for sampling and volume production. Pricing starts at $12.00 each for Microchip’s DM870A Wi-Fi network media processor chipset, combined with the JB3.2 software, in quantities of 25,000 units per year. For more information on Microchip’s JukeBlox technology, contact any Microchip sales representative or authorized worldwide distributor, or visit http://www.microchip.com/get/KLB2.
Resources
High-res Photo Available Through Flickr or Editorial Contact (feel free to publish): http://www.microchip.com/get/8VWM
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/BPDQ
- Twitter: http://www.microchip.com/get/GHXQ
- Facebook: http://www.microchip.com/get/T8N2
- YouTube: http://www.microchip.com/get/3WTM
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, mixed-signal, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/WND7.
Note: The Microchip name and logo, and JukeBlox are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: JukeBlox, music streaming, audio streaming, connectivity solution, network media module, network media processor, media networking, WiFi streaming
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/KLB2
Source: Microchip Technology Inc.
Released January 9, 2013