Microchip Expands mTouch™ Sensing Portfolio with Turnkey Controllers for Multitouch, Proximity Detection and Haptic Feedback
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog, mixed-signal and Flash-IP solutions, today announced the expansion of its mTouch™ Sensing Solutions portfolio, with four turnkey controllers for multitouch projected-capacitive touchscreens and touchpads, proximity detection, and haptic touch feedback.
The MTCH6301 is a turnkey projected-capacitive touch controller that makes it easy for designers to add popular multitouch and gesture interfaces—eliminating the learning curve and time of creating a design from scratch. This controller’s sophisticated combination of Self and Mutual capacitive scanning for XY touchscreens and touchpads enables a host of features, including: single and dual-touch drawing, the reporting of 11 single-finger gestures and the detection of up to 10 touches. The MTCH6301 supports sensor designs with up to 13 x 18 channels and cover lenses up to 5 mm. Additionally, Microchip offers its free “Projected Capacitive Configuration Utility” with automatic tuning, enabling fast customization for different screen sizes and top-layer thicknesses. Microchip also provides designers with the firmware library, so they can make further customizations.
The MTCH101 and MTCH112 are turnkey controllers in small packages that provide an easy way to add robust proximity detection with a range of up to 8 inches. Additionally, these low-cost controllers maximize battery life with power consumption as low as 5 microamps. The MTCH101/112 also provide advanced noise avoidance and cancelling technology, and can operate standalone or connected to any microcontroller via I2C™, making it easy to add touchless operation or user detection to any design. This is particularly useful for mobile devices that must reduce 3G/4G transmission power in the presence of a user, in order to pass the FCC’s Specific Absorption Rate (SAR) test. Proximity detection also enables reduced system power consumption, by inducing sleep when no users are present.
The MTCH810 is the first in a family of controllers based on Microchip’s license of Immersion’s TouchSense® haptic feedback technology. This controller enables the easy addition of haptic tactile feedback to any capacitive-touch button or slider interface. It integrates a single-channel haptic driver output with an industry-standard I2C slave interface that connects to any MCU—all in a small, 8-pin package. Designers can differentiate their products while improving the user experience by utilizing any of the 14 different haptic effects that are pre-programmed into the MTCH810 controller, such as single vibrate and double vibrate.
“We’re pleased to be working with Microchip to support the increasing demand for haptic-enabled touch experiences,” said Immersion’s Sr. Vice President of Sales & Marketing, Dennis Sheehan. “By incorporating Immersion’s tactile feedback technology into Microchip’s touch solutions, OEMs and designers will be able to easily create more intuitive and compelling user interfaces with haptics.”
Pricing & Availability
The MTCH6301 projected-capacitive controller is available in 44-pin QFN and TQFP packages, and pricing starts at $1.86 each, in 10,000-unit quantities. The MTCH101/112 proximity-detection controllers start at $0.25 each, in 10,000-unit quantities. The MTCH101 is offered in a 6-pin, SOT-23 package, while the MTCH112 is packaged in the 8-pin SOIC and DFN. The MTCH810 haptic-feedback controller is available in a 3x3 mm, 8-pin DFN package, and pricing starts at $0.87 each, in 10,000-unit quantities.
All of four of these controllers are available today for sampling, and volume production is expected in December. For additional information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/LFNJ. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
Resources
High-res Images Available Through Flickr or Editorial Contact (feel free to publish):
- MTCH6301 Photo: http://www.microchip.com/get/3HRU
- MTCH810 Photo: http://www.microchip.com/get/85BA
- MTCH101/112 Photo: http://www.microchip.com/get/RRU2
Follow Microchip:
- RSS Feed for Microchip Product News: http://www.microchip.com/get/6LF8
- Twitter: http://www.microchip.com/get/FWG1
- Facebook: http://www.microchip.com/get/LTUD
- YouTube: http://www.microchip.com/get/K2LA
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog, mixed-signal and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/8FTB.
Note: The Microchip name and logo is a registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. mTouch is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Tags / Keywords: Touch, Projected Capacitive, PCap, Gestures, Multi-touch, Interface, Touch Screen, mTouch, Haptics, Immersion, Tactile, Proximity, Low Power, Prox, Turnkey
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/LFNJ
Source: Microchip Technology Inc.
Released November 20, 2012