Microchip Further Expands Stand-Alone Real-Time Clock Calendar Device Family
New, Low-Cost I2C™ RTCC Device Includes 64 Bytes SRAM, Digital Trimming Circuit That Can Compensate Up to 11 Seconds Per Day for Crystal Error
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced the expansion of its stand-alone Real-Time Clock Calendar (RTCC) family with the I2C™ MCP7940M RTCC device. This new device is designed for the price-competitive consumer products market, and includes 64 Bytes of SRAM as additional scratchpad memory, as well as a digital-trimming circuit that can compensate up to 11 seconds per day for crystal error. The MCP7940M devices provide accurate timekeeping at a low cost for applications in the home-appliance (e.g., microwaves, washing machines, dryers, ovens, thermostats); audio/video (e.g., radios, televisions, set-top boxes, digital recorders); and consumer-electronic markets (e.g., printers, network routers, cameras), among others.
Following the launches of Microchip’s stand-alone I2C MCP79410 and SPI MCP795WXX/BXX RTCC devices in 2010 and 2011, respectively, the MCP7940M device has a simple feature set that meets the needs of the high-volume segment of the RTCC device market. Microchip now has stand-alone RTCC devices for the low, mid and upper-mid ranges of this market. The on-chip digital trimming circuit has a wide trimming range of +/-127 ppm, enabling designers to select lower-quality crystals for their designs to reduce overall system costs.
“After receiving many customer requests for low-end real-time clocks and conducting our own analysis of this market, we developed the MCP7940M RTCC device,” said Randy Drwinga, vice president of Microchip’s Memory Products Division. “By offering a price-competitive RTCC that also includes 64 Bytes of SRAM and a digital-trimming circuit for higher accuracy, we believe that our solution will have a distinct advantage over the competition.”
Development Support
Microchip’s MCP79410 RTCC PICtail™ Plus Daughter Board (part # AC164140, $45) is available, today. The board works with Microchip’s Explorer 16 Development Board (part # DM240001, $129.99), PIC18 Explorer Board (part # DM183032, $99.99), PICkit™ Serial Analyzer (part # DV164122, $49.99), and XLP 16-bit Development Board (part # DM240311, $59.99).
Packaging, Pricing & Availability
The MCP7940M RTCC is available today in 8-pin MSOP, PDIP, SOIC, TSSOP and 2 mm x 3 mm TDFN packages. Pricing starts at $0.45 each, in 10,000-unit quantities. Samples can be ordered today, at http://www.microchip.com/get/G8UL. Volume-production quantities of the devices can be purchased today, at microchipDIRECT (http://www.microchip.com/get/E1NA). For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/SS5J. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/X64G).
Note: The Microchip name and logo are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. PICtail is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res Photo and Block Diagram available through editorial contact
or Flickr (feel free to publish):
Photo http://www.microchip.com/get/HTFQ
Block
Diagram http://www.microchip.com/get/R3WA
Tags / Keywords: Real-Time Clock, Real-Time Clock Calendar, Real Time Clock, RTCC
RSS Feed for Microchip Product News: http://www.microchip.com/get/A8D3
Microchip Technology Inc.
Editorial Contact:
Michelle
Ragsdale, 480-792-4111
michelle.ragsdale@microchip.com
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/SS5J
Source: Microchip Technology Inc.
Released March 5, 2012