Microchip Upgrades Enhanced Core dsPIC33E and PIC24E Devices to 70 MIPS
Additionally, Three New 64-pin Motor Control and General-Purpose Devices Added to Family
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced the upgrade of its formerly 60 MIPS enhanced-core dsPIC33E Digital Signal Controllers (DSCs) and PIC24E microcontrollers (MCUs) to 70 MIPS performance. The devices feature 536 KB Flash memory and 52 KB RAM, greater I/O capabilities, a USB 2.0 OTG interface, and enhanced motor-control, graphics, audio and real-time embedded-control capabilities. Additionally, the family has been expanded with the release of three new non-USB 64-pin devices that are fully compatible with Microchip’s entire portfolio of dsPIC33F DSCs and PIC24H/PIC24F MCUs, software libraries and tools, providing a solid growth path for current customers.
The upgraded 70 MIPS motor-control DSCs enable designers to expand motor-control system performance in high-end industrial and commercial applications. These devices include Microchip’s industry-leading motor control PWM peripherals, enabling the generation of PWM waveforms needed to control virtually any motor, such as servos, and running dual three-phase motors in parallel. A new dead-time compensation feature reduces software overhead. Additionally, the USB 2.0 OTG peripheral enables connections to a PC, Flash drive and other USB-enabled devices, and 70 MIPS performance means the new DSCs and MCUs support computer-interfaced applications. Three on-chip analog comparators further reduce system cost and the number of external components required. These capabilities, coupled with the family’s high integration, make them some of the most capable motor control devices on the market.
“Upgrading our recently-introduced portfolio of dsPIC33E and PIC24E devices to 70 MIPS allows our customers to benefit from higher performance at no extra cost,” said Sumit Mitra, vice president of Microchip’s High-Performance Microcontroller Division. “The three new 64-pin devices with 536 KB Flash memory facilitate applications needing larger Flash and RAM memories, while still fitting into a small 9 mm x 9 mm QFN footprint.”
Development Tool Support
Designers can use the same tools that they did for the dsPIC33 and PIC24 “E” families. This includes the dsPIC33E USB Starter Kit (part # DM330012, $65) and the PIC24E USB Starter Kit (part # DM240012, $65), which are both available today. These starter kits can be used for stand-alone development, and also work with an assortment of Microchip’s daughter boards, such as its Multimedia Expansion Board (part # DM320005), which enables the development of high-impact user interfaces.
Additionally, there are several Plug-In Modules (PIMs) available for Microchip’s Explorer 16 Development Board and motor-control development kits, including the dsPICDEM™ MCHV (part # DM330023), dsPICDEM MCLV (part # DM330021) and dsPICDEM MCSM (part # DM330022) kits. PIMs include the dsPIC33E 100-pin PIM for Motor-Control, General-Purpose and Graphics applications (part # MA330025-1, $25); PIC24E 100-pin PIM for General-Purpose and Graphics Applications (part # MA240025-1, $25); dsPIC33E 144-pin PIM for General-Purpose and Graphics Applications (part # MA330025-2, $30); dsPIC33E 144-pin PIM for Motor-Control Applications (part # MA330025-3, $40); and PIC24E 144-pin PIM for General-Purpose and Graphics Applications (part # MA240025-2, $30). The dsPIC33E Dual Motor Control PIM (part # MA330027, $175) enables designers to simultaneously control two motors using one dsPIC33E DSC.
Packaging, Pricing & Availability
The 70 MIPS dsPIC33E and PIC24E devices are available in 64-pin QFN and TQFP packages, a 100-pin TQFP package, a 121-pin BGA package, and 144-pin LQFP and TQFP packages. Pricing starts at $4.98 each, in 10,000-unit quantities. Samples and volume-production quantities can be ordered today. For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/get/9FFK. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/0SRT).
Note: The Microchip name and logo, dsPIC, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. dsPICDEM is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res Photos and Block Diagram available through editorial contact or Flickr (feel free to publish):
Photo http://www.microchip.com/get/9VRV
Block
Diagram http://www.microchip.com/get/SUN2
Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, dsPIC, DSC, Digital Signal Controller, motor control
RSS Feed for Microchip Product News: http://www.microchip.com/get/TW3N
Microchip Technology Inc.
Editorial Contact:
Michelle
Miley, 480-792-4111
michelle.miley@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/9FFK
Source: Microchip Technology Inc.
Released February 27, 2012