Microchip Wins Best of Electronic Design Award for 8-bit MCUs With Configurable Logic in 6- to 20-pin Packages
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced that its 8-bit PIC10F32X and PIC1XF150X microcontroller (MCU) families won a 2011 “Best of Electronic Design” Award in the Digital category, from Electronic Design Magazine. The general-purpose PIC10F(LF)32X and PIC1XF(LF)150X MCUs include integrated configurable logic in 6- to 20-pin packages. The MCUs feature a new Configurable Logic Cell (CLC) peripheral that provides software control of combinational and sequential logic, which increases the on-chip interconnection of peripherals and I/Os, thereby reducing external components, saving code space and enabling applications for microcontrollers that didn’t exist before. These new MCUs allow designers to enhance the functionality, reduce the design size, and decrease the cost and power consumption of products in the appliance, automotive, consumer, and industrial markets, among others.
Click here to view related videos (feel free to embed on your site): http://www.microchip.com/get/W9C3.
“Microchip continues to enable designers to do more with less,” said Bill Wong, Electronic Design’s Digital Editor. “With their combination of configurable logic in 6- to 20-pin packages at a low cost, the PIC10F32X and PIC1XF150X MCUs enable designers to create higher-performing applications while keeping costs low.”
“The PIC10F32X is a great family of parts, and we’re honored to receive this award,” said Steve Drehobl, vice president of Microchip’s Security, Microcontroller and Technology Development Division. “The unmatched combination of unique functionality, power consumption, size, and low cost that the PIC10F32X and PIC1XF150X MCUs provide enables designers to innovate, and create new applications for microcontrollers.”
In addition to the CLC, the PIC10F32X and PIC1XF150X MCUs feature Complementary Waveform Generator (CWG) and Numerically Controlled Oscillator (NCO) peripherals. The CWG works with multiple peripherals to generate complementary waveforms with dead-band control and auto shutdown, which provides improved switching efficiencies. The NCO peripheral enables linear frequency control and high resolution, which is required for applications such as lighting-ballast, tone-generation and other resonant-control circuits. Additionally, the MCUs feature low power consumption, with currents of less than 30 µA/MHz in active mode, and less than 20 nA in sleep; as well as on-chip 16 MHz oscillator, Analog-to-Digital Converter (ADC), and up to 4 Pulse-Width Modulation peripherals. An integrated temperature-indicator module enables low-cost temperature measurements.
For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip’s Web site at http://www.microchip.com/wwwproducts/Devices.aspx?dDocName=en552961. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip’s authorized distribution partners.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/XW3D).
Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res Photos and Block Diagram available through editorial contact or Flickr (feel free to publish):
PIC10F32X Block Diagram http://www.microchip.com/get/JC5E
PIC1XF150X Block Diagram http://www.microchip.com/get/W7NC
Photo http://www.microchip.com/get/TEWP
Videos (feel free to embed on your site): http://www.microchip.com/get/W9C3
Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, configurable logic, low pin count, 6-pin
RSS Feed for Microchip Product News: http://www.microchip.com/get/808U
Microchip Technology Inc.
Editorial Contact:
Michelle
Miley, 480-792-4111
michelle.miley@microchip.com
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/AR52
Source: Microchip Technology Inc.
Released February 1, 2012