Microchip Launches Embedded Code Source, an Application Store and Social Community for Downloading and Rating Free PIC® MCU Code
Site Includes Free Third-Party Code; Accelerates Code Development and Time to Market
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced the Embedded Code Source (http://www.microchip.com/get/R0BA), an application store for the embedded community that provides free software and firmware for PIC® microcontrollers, along with the ability to rate and review each download. This interactive site includes free code from both Microchip and its large network of third-party developers, who are also available for expert advice and contract programming.
Watch a video about the Embedded Code Source (feel free to post): http://www.microchip.com/get/CU92
Recent surveys have shown that a majority of embedded designers consider software tools to be a critical factor in choosing a processor, and that the largest portion of most development teams is comprised of software engineers. These trends, combined with the increasing popularity of open-source and freeware code, point to the need for more embedded software resources. The Embedded Code Source combines Microchip’s extensive code repository with those of its large third-party network to provide a comprehensive, free and easily searchable resource for the embedded community.
“Microchip is continually looking for ways to help customers get to market faster,” said Ken Pye, Microchip’s vice president of Worldwide Applications. “With engineering budgets and schedules under constant pressure, software engineers need fast access to code that they can use, new ideas, and feedback on what others have found beneficial. Patterned after popular mobile-application stores, the new Embedded Code Source fulfills this need.”
Designers can begin downloading from the Embedded Code Source today, by browsing its list of intuitive categories or performing a keyword search at http://www.microchip.com/get/R0BA.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Arizona, Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/0FX4.
Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Inc. in the USA and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res Photo Available Through Flickr or Editorial Contact (feel free to publish): http://www.microchip.com/get/Q7SW
Video Available Through YouTube or Editorial Contact (feel free to post): http://www.microchip.com/get/CU92
Tags / Keywords: Source Code, Software Library, PIC Code, Free Code, Code Examples, Search, Review, Download
RSS Feed for Microchip Corporate News: http://www.microchip.com/get/BXRA
Microchip Technology Inc.
Editorial Contact:
Eric
Lawson, 480-792-7182
eric.lawson@microchip.com
or
Reader
Inquiries:
1-888-624-7435
http://www.microchip.com/get/R0BA
Source: Microchip Technology Inc.
Released October 3, 2011