Microchip and Digilent Create Network and Basic I/O Shields, Support Resources for the chipKIT™ and Arduino™ Community
Shields and Support Resources Enable Hobbyists and Academics to Add More Features and Functionality to Projects, Even If They Are Not Engineers
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, and Digilent, Inc. today announced expanded capabilities for the 32-bit PIC32 microcontroller-based chipKIT™ Development Platform for the Arduino™ community. First, the companies unveiled two shields for the chipKIT platform—the chipKIT Basic I/O and Network Shields. Secondly, new online support resources for the community are now available, including software library support for Ethernet, CAN and USB, as well as an online chipKIT forum (http://www.microchip.com/get/TGRC) and wiki (http://www.microchip.com/get/6ST7). The shields and online support resources enable users to take advantage of the high-performance, 32-bit PIC® microcontroller-based chipKIT development platform to add more features and functionality to their projects, even if they are not engineers.
A video can be viewed at the following link (feel free to embed on your site): http://www.microchip.com/get/UVRQ.
The chipKIT development platform is a 32-bit Arduino solution that enables hobbyists and academics to easily and inexpensively integrate electronics into their projects, even if they do not have an electronic-engineering background. The platform consists of two PIC32-based development boards and open-source software that is compatible with the Arduino programming language and development environment. The chipKIT hardware is compatible with existing 3.3V Arduino shields and applications, and can be developed using a modified version of the Arduino IDE and existing Arduino resources, such as code examples, libraries, references and tutorials. The chipKIT Basic I/O Shield (part # TDGL005) announced today is compatible with the chipKIT Uno32™ and Max32™ boards, and offers users simple push buttons, switches, LEDs, I2C™ EEPROM, I2C temperature sensor, and a 128 x 32 pixel organic LED graphic display. The chipKIT Network Shield (part # TDGL006) enables users to use the chipKIT Max32™ development board to implement 10/100 Ethernet, USB OTG and CAN communications.
“The introduction of these two new shields for the chipKIT platform demonstrates Microchip’s and Digilent’s commitment to the Arduino community,” said Fred Eady, hobbyist and editor with Nuts & Volts and SERVO Magazines. “Not only will users have additional I/O functionality with the chipKIT Basic I/O Shield, they will be able to integrate advanced communications such as Ethernet, CAN and USB into their projects with the Network Shield.”
“We’re excited to continue supporting the academic and hobbyist communities with the expanded capabilities of and support for the chipKIT development platform,” said Derek Carlson, Microchip’s vice president of development tools.
Clint Cole, president of Digilent, Inc., said, “These new shields and online support resources open new opportunities for industry, hobbyists and academics to do more with their chipKIT-based projects, as well as collaborate and share ideas.”
Pricing & Availability
The chipKIT Basic I/O Shield (part # TDGL005, $37.99) and chipKIT Network Shield (part # TDGL006, $54.99) can be purchased today, at http://www.microchip.com/get/0DLG and http://www.microchip.com/get/9LQX. For more information, please visit the Digilent Web site (http://www.microchip.com/get/0DLG), or contact Joe Harris at joe@digilentinc.com, or (509) 334-6306. More information is also available on Microchip's Web site, at http://www.microchip.com/get/9LQX.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/CF4U).
About Digilent, Inc.
Digilent, Inc. is a leader in providing academic and research solutions to high-end electronics fields. Their headquarters are in Pullman, Washington, with offices in Taiwan, China, and Romania. Currently, over 1,000 universities, training centers and research laboratories in more than 70 countries use Digilent products and services. For more information, please visit the Digilent Web site (http://www.microchip.com/get/1JSX).
Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. chipKIT is a trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.
Video (feel free to embed on your site): http://www.microchip.com/get/UVRQ
High-res photos available through editorial contact or Flickr (feel
free to publish):
chipKIT Basic I/O Shield
http://www.microchip.com/get/2QSU
chipKIT Network Shield
http://www.microchip.com/get/KJ3B
Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, Arduino, chipKIT, hobbyist, academic, open source, network shield, I/O shield
RSS Feed for Microchip Product News: http://www.microchip.com/get/XQ7M
Microchip Technology Inc.
Editorial Contact:
Michelle
Ragsdale, 480-792-4111
michelle.ragsdale@microchip.com
Reader
Inquiries:
1-509-334-6306
http://www.microchip.com/get/0DLG
Source: Microchip Technology Inc.
Released August 22, 2011