Microchip Unveils Advanced Development Kit for High-Quality Digital Audio Applications
32-bit Microcontroller-based Dev Kit Provides Complete Solution for the Development of 24-bit Audio and Speech Applications With Record, Playback and Mixing Capabilities
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced a 32-bit microcontroller (MCU)-based development kit for the creation of high-quality, 24-bit audio applications. The Audio Development Board for PIC32 MCUs features an 80 MIPS PIC32 MCU, a 24-bit Wolfson audio codec, a two-inch color LCD Display, a USB interface, and an onboard microphone. Supported by Microchip's free software libraries, the kit provides a perfect solution for the development of speech and audio recording and playback products. Target applications include docks for portable audio players, home-entertainment systems and automotive sound systems.
The 80-MIPS PIC32MX795F512L MCU on the audio development board features 512 KB Flash and 128 KB RAM, providing plenty of processing power and memory to decode, analyze and play back audio and speech. Libraries are available for speech recording and playback, as well as MP3 music decoding applications. Additionally, an audio Sample Rate Conversion (SRC) library for 33 kHz, 44.1 kHz and 48 kHz is also supported, which enables developers to reduce component costs for playback solutions. There are also libraries available for managing the USB interface and driving the on-board color LCD display, which features 16-bit color images. For those developers who are enrolled in the Apple(R) Made For iPod (MFi) Licensing Program, the kit also interfaces to Microchip's accessory development platform for iPod(R) and iPhone(R).
"The Audio Development Board for PIC32 MCUs offers a complete platform that doesn't break the budget for high-quality audio development," said Sumit Mitra, vice president of Microchip's High-Performance Microcontroller Division. "The board also includes an interface for use with our accessory development platform for iPod and iPhone, enabling expansion to support these popular devices."
Packaging, Pricing & Availability
The Audio Development Board for PIC32 MCUs (part # DM320011) is available today, for $149.99 at microchipDIRECT (http://www.microchip.com/get/LJEC). For MFi licensees, the Digital Audio Development Kit for PIC32 MCUs (part # DM320411) adds the accessory development platform for iPod and iPhone. This kit will be available by September to MFi licensees via Apple's authorized distributor. For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at: http://www.microchip.com/get/ELSA.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/K1W8).
Note: The Microchip name and logo, and PIC, are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. iPhone and iPod are trademarks of Apple Inc., registered in the United States and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res photos available through editorial contact or Flickr (feel free to publish):
Audio Development Board for PIC32 MCUs
http://www.microchip.com/get/JHUK
Digital Audio Development Kit for PIC32 MCUs
http://www.microchip.com/get/T6K4
Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, audio, MP3, development kit, iPod, iPhone
RSS Feed for Microchip Product News: http://www.microchip.com/get/DTVE
Source: Microchip Technology Incorporated
Released July 18, 2011