Microchip and Digilent Launch First Arduino(TM) Compatible 32-bit Microcontroller Development Platform

Platform Includes Dev. Boards, Open-Source Software; 32-bit Performance and Low Cost Enable Hobbyists & Academics Of All Disciplines to Integrate Electronics Into Projects

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ:MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, and Digilent, Inc. today launched the first 32-bit-microcontroller-based, open-source development platform that is compatible with Arduino(TM) hardware and software. Designed and manufactured by Digilent, a Microchip Authorized Design Partner, the chipKIT(TM) platform is the first and only 32-bit Arduino solution in the industry to enable hobbyists and academics to easily, and inexpensively, integrate electronics into their projects, even if they do not have an electronic-engineering background. The platform consists of two PIC32-based development boards and open-source software that is compatible with the Arduino programming language and development environment, thanks to the incredible work done by Mark Sproul and Rick Anderson through Fair Use Building and Research Labs. The chipKIT hardware is compatible with existing 3.3V Arduino shields and applications, and can be developed using a modified version of the Arduino IDE and existing Arduino resources, such as code examples, libraries, references and tutorials. The platform provides an unprecedented level of features for the Arduino community, and four times the performance of any existing Arduino solution at a low price--the boards start at just $26.95 each. A video can be viewed online at (feel free to embed on your site): http://www.microchip.com/get/D268.

A video can be viewed online at (feel free to embed on your site): http://www.microchip.com/get/D268 (Photo: Business Wire)

Hobbyists and academics from many disciplines, such as mechanical engineering, computer science and even art, want easy-to-use, low-cost solutions for creating projects. The PIC32-based chipKIT boards enable 80 MHz performance, and provide up to 512 KB Flash, with up to 128 KB RAM. The boards feature connectivity peripherals, including Ethernet, CAN, and USB (Full-Speed Host, Device and OTG); plus peripherals such as multiple timers, a 16-channel 1 MSPS Analog-to-Digital Converter (ADC), two comparators, and multiple I2C(TM), SPI, and UART interfaces. Not only is chipKIT the first Arduino-compatible platform to provide 32-bit performance, but Microchip's PIC32 microcontroller is also the highest performance 32-bit microcontroller in its class, featuring the industry-leading MIPS32(R) M4K(R) core from MIPS Technologies, Inc.

A tremendous software engineering effort has been invested to ensure maximum compatibility with existing Arduino shields, applications and courseware. The Arduino programming environment has been modified and extended so that it supports the PIC32-based chipKIT boards, as well as traditional Arduino boards. The Arduino standard libraries have been also been modified to support chipKIT boards and traditional Arduino boards. All of this work has been contributed back to the open-source Arduino community. Aside from a small number of shields that require 5V operation, many existing Arduino hardware and software sketches are compatible with the chipKIT platform, without modification.

"Students, educators and hobbyists, with or without electronic-engineering backgrounds, are looking for inexpensive solutions that will enable them to easily integrate electronics into their projects," said Derek Carlson, Microchip's vice president of Development Systems. "The chipKIT boards and software meet these needs, providing far more features, performance and functionality than any other Arduino solution on the market, at a low cost."

"The chipKIT platform is the first and only 32-bit solution of its kind in the industry," said Clint Cole, president of Digilent, Inc. "Academics and hobbyists can plug the boards into their design, download the open-source software and have their project up and running in minutes."

Art Swift, vice president of marketing and business development for MIPS Technologies, Inc., said, "The chipKIT platform enables academia and hobbyists to experience the superior performance efficiency of the MIPS(R) architecture, which many professional electronics designers have preferred for years."

Board-Specific Features, Pricing & Availability

The chipKIT Uno32(TM) (part # TDGL002) development board is a clone of the Arduino Uno board, and features 128 KB Flash program memory and 16 KB RAM, with two each of the I2C, SPI and UART peripherals. This board is priced at $26.95 each. A clone of the Arduino Mega board, the chipKIT Max32(TM) (part # TDGL003) development board features 512 KB Flash program memory and 128 KB RAM, with USB, CAN and Ethernet communication, as well as 5 each I2C, 4 each SPI, and 6 each UART peripherals. The chipKIT Max32 board is priced at $49.50 each. Both chipKIT boards can be ordered today, at http://www.microchip.com/get/TDD2. Additionally, the open-source software for both boards is available today at http://www.microchip.com/get/TDD2. chipKIT Network and I/O Shields are expected to be available in June 2011.

For more information, please visit the Digilent Web site (http://www.microchip.com/get/TDD2), or contact Joe Harris at joe@digilentinc.com, or (509) 334-6306. More information is also available on Microchip's Web site, at http://www.microchip.com/get/SDTW.

About Digilent, Inc.

Digilent, Inc. is a leader in providing academic and research solutions to high-end electronics fields. Their headquarters are in Pullman, Washington, with offices in Taiwan, China, and Romania. Currently, over 1,000 universities, training centers and research laboratories in more than 70 countries use Digilent products and services. For more information, please visit the Digilent Web site (http://www.microchip.com/get/VUSS).

About Microchip Technology

Microchip Technology Inc. (NASDAQ:MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/A53X).

Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. chipKIT is a trademark of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

Video (feel free to embed on your site): http://www.microchip.com/get/D268

High-res photos available through editorial contact or Flickr (feel free to publish):

chipKIT Uno32 photo http://www.microchip.com/get/0WUW

chipKIT Max32 photo http://www.microchip.com/get/5E6V

Stylized product photo http://www.microchip.com/get/AF77

Tags / Keywords: Arduino, Microchip, MCHP, PIC, microcontroller, MCU, development tool, open source, electronic hobbyist, electronics

RSS Feed for Microchip Product News: http://www.microchip.com/get/9H21

Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6733461&lang=en


    Source: Microchip Technology Inc.