Microchip Introduces Low-Cost 8-bit PIC(R) Microcontrollers With eXtreme Low Power Technology and Integrated LCD Control

MCUs Enable Low-Cost LCD Control With Industry-Leading Low Power

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced an expansion of its 8-bit segmented LCD microcontroller (MCU) family with five new devices--the PIC16LF1902/3/4/6/7 (PIC16LF190X) MCUs. The PIC16LF190X family supports many general-purpose applications and enables the implementation of LCD into low-power and cost-sensitive designs, such as security tokens, smart cards, medical devices, home appliances, key fobs or any application involving a segmented LCD. Featuring eXtreme Low Power (XLP) technology for sleep currents down to 20 nA, and a typical active current of 35 microamperes per MHz, the MCUs extend battery life, while maintaining accurate timing with a RTC and driving a segmented LCD.

Utilizing Microchip's Enhanced Mid-range architecture, the PIC16LF190X family provides fundamental features and performance without burdening customers with the cost of unused peripherals. These MCUs provide an optimized feature set, including up to 14 KB of Flash program memory, up to 512 bytes of RAM, up to 14 10-bit Analog-to-Digital Converter (ADC) channels, serial communication, temperature indicator and the capability to drive up to 116 LCD segments. With the addition of XLP technology for extended battery life, and capabilities such as utilizing the integrated temperature indicator to provide crystal-accuracy compensation, low-power RTC support and low voltage-detect support utilizing the internal ADC and voltage reference, the MCUs enable low-cost LCD solutions for a multitude of portable devices.

"With industry-leading low power and an optimized feature set, the PIC16LF190X family is designed for any low-power segmented LCD or general-purpose application," said Steve Drehobl, vice president of Microchip's Security, Microcontroller & Technology Development Division.

Development Support

The PIC16LF190X MCUs are supported by the F1 Evaluation Kit (part # DM164132, $69.99) and Platform (part # DM164130-1, $39.99), as well as the PICkit(TM) 3 In-Circuit Debugger (part # PG164130, $44.95). Designers can also utilize the full suite of MPLAB(R) development tools, including the MPLAB IDE, MPLAB ICD3, REAL ICE(TM) In-Circuit Emulator and HI-TECH C(R) compiler for PIC10/12/16 MCUs. All of these tools can be purchased today, at http://www.microchip.com/get/P5NK.

MCU Packaging, Pricing & Availability

The PIC16LF1902, PIC16LF1903 and PIC16LF1906 MCUs are all available in 28-pin SPDIP, SOIC, SSOP, and 4 mm x 4 mm UQFN and die packages. The PIC16LF1904 and PIC16LF1907 MCUs are available in 40-pin PDIP, 5 mm x 5 mm UQFN and die packages, as well as a 44-pin TQFP. Pricing starts at $0.75 each, in 10,000-unit quantities. Samples are available today, at http://www.microchip.com/get/FKLT. Volume-production quantities can be ordered today, at microchipDIRECT (http://www.microchip.com/get/P5NK). For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at http://www.microchip.com/get/MRHX. To purchase products mentioned in this press release, go to microchipDIRECT or contact one of Microchip's authorized distribution partners.

About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/UPT9).

Note: The Microchip name and logo, HI-TECH C, MPLAB and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. PICDEM, PICkit, and REAL ICE are trademarks of Microchip Technology Inc. in the U.S.A., and other countries. All other trademarks mentioned herein are the property of their respective companies.

High-res photo and block diagram available through editorial contact or Flickr (feel free to publish):

Photo
http://www.microchip.com/get/BGDG

Block Diagram
http://www.microchip.com/get/DVDL

Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, LCD microcontroller

RSS Feed for Microchip Product News: http://www.microchip.com/get/31TP


    Source: Microchip Technology Inc.