USB Microcontrollers From Microchip Feature eXtreme Low Power Consumption in 28- and 44-pin Packages

PIC(R) Microcontrollers Offer Up to 128 KB Flash Memory and 4 KB RAM--Plenty of Space for Free USB Stack and Application Code

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today expanded its 8-bit and USB microcontroller (MCU) lines with the PIC18F47J53. Featuring XLP technology for eXtreme Low Power Consumption, the new MCU provides up to 128 KB Flash program memory and 4 KB RAM, offering plenty of code space for Microchip's free USB stack, and for application code. The MCU features full-speed USB 2.0 capability, enabling applications that can perform remote field upgrades, download usage data and connect to diagnostic equipment, which results in lower costs and more flexibility for the end user. The integrated mTouch(TM) sensing capability enables easy implementation of capacitive touch sensing user interfaces, while XLP technology drastically reduces the amount of power consumed, helping to extend battery life. By having USB integrated on this XLP family of MCUs, there is no need to sacrifice power consumption just to have USB.

Many portable applications, such as smart-card readers, need to occasionally connect to a PC or another portable device via USB. The full-speed USB 2.0 capability of the PIC18F47J53 MCU enables this, and Microchip offers a free smart card library, within its free USB stack. An on-chip 12-bit Analog-to-Digital Converter delivers the accuracy required for many advanced sensor, instrumentation and measurement applications. With multiple PWMs, timers and SPI channels with DMA, the PIC18F47J53 MCU is well suited for portable consumer devices, medical devices, and other applications requiring low power consumption and USB connectivity.

"The PIC18F47J53 family broadens our portfolio of cost-effective XLP products with integrated USB, for portable applications that need to share data," said Mitch Obolsky, vice president of Microchip's Advanced Microcontroller Architecture Division.

Obolsky continued, "The MCU offers a fully compatible memory extension to our popular PIC18F46J50 USB family, serving a wide spectrum of applications, such as handheld medical devices and speaker accessories for iPod(R)."

Development Tool Support

Microchip also announced the PIC18F47J53 Full-Speed USB Demo Board (part # MA180029, $45), today. This board can be used stand-alone or as a plug-in to the PIC18 Explorer Board (part # DM183032, $99.99). Additionally, designers can use Microchip's complete suite of standard development tools with the new MCUs, including the user-friendly and free MPLAB(R) IDE and corresponding suite of emulators, programmers and development boards, along with the MPLAB C or HI-TECH C(R) compiler for PIC18 MCUs. For more information, visit the Microchip development tools Web site (http://www.microchip.com/get/RRTJ).

Packaging, Pricing & Availability

The PIC18F27J53 MCU is available in 28-pin QFN, SOIC, SPDIP, and SSOP packages. The PIC18F47J53 MCU is available in 44-pin QFN and TQFP packages. Pricing starts at $2.31 each, in 10,000-unit quantities. Samples can be ordered today, at http://www.microchip.com/get/0HW6. Volume-production quantities can be purchased today, at http://www.microchip.com/get/1Q1Q. For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at http://www.microchip.com/get/JD32.

About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog, and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip Web site at http://www.microchip.com/get/HJB0.

Note: The Microchip name and logo, HI-TECH C, MPLAB, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. mTouch is a trademark of Microchip Technology Inc. in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

High-res Photos and Block Diagram available through editorial contact or Flickr (feel free to publish):

Photo

http://www.microchip.com/get/FTKT

Block Diagram

http://www.microchip.com/get/LCKS

Photo of PIC18F47J53 PIM:

http://www.microchip.com/get/X6TH

Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, PIC18F47J53, USB, capacitive touch sensing, MPLAB, XLP, eXtreme Low Power, high memory, mTouch, 12-bit ADC

RSS Feed for Microchip Product News:

http://www.microchip.com/get/LNXS


    Source: Microchip Technology Inc.