Low-Power, Small Form Factor Op Amps from Microchip Help Extend Battery Life
      Op Amps Feature Low Quiescent Current of 45 microamperes at 1 MHz;
Available
      in Space-Saving SC-70 and SOT-23 Packages
    
CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller, analog and Flash-IP solutions, today announced the MCP6401/2/4 Operational Amplifiers (Op Amps), which add to Microchip's general-purpose op amp portfolio by providing lower power consumption in small packages. Featuring quiescent current of just 45 microamperes with a Gain Bandwidth Product (GBWP) of 1 MHz, the MCP6401/2/4 op amps complement Microchip's eXtreme Low Power PIC(R) microcontrollers (MCUs), helping to extend battery life in a variety of consumer (e.g., music players, appliances and gaming consoles); industrial (e.g., barcode scanners and gas meters); automotive (e.g., signal conditioning for proximity and tire-pressure-measurement sensors); and medical applications (e.g., glucometers and portable patient-monitoring devices), among others.
Additional features include a maximum offset voltage of +/-4.5 mV and a supply-voltage range of 1.8V to 6V over the extended temperature range of - 40 C to + 125 C. The op amps are unity gain stable and feature Rail-to-Rail Input and Output operation for better performance across the entire voltage range.
"Customers often cite low current consumption and small form factor as being the most important requirements when designing battery-powered, portable and other applications," said Bryan J. Liddiard, vice president of marketing with Microchip's Analog and Interface Products Division. "The MCP6401/2/4 op amps address both of these needs, reinforcing Microchip's leadership as the low-power analog product supplier."
Namrata Pandya, product marketing engineer with Microchip's Analog and Interface Products Division, continued, "With advantages such as the low operating voltage range and low power consumption in space-saving packages, the MCP6401/2/4 op amps provide a good cost-to-performance ratio, while helping system engineers meet tight power budgets and save valuable board space."
Development Support
PCB footprints and schematic symbols are expected to be available in September 2010 from Microchip's Web site at http://www.microchip.com/get/G98J. The downloads will be available in a neutral format that can be exported to the leading EDA CAD/CAE design tools, using the Ultra Librarian Reader from Accelerated Designs Incorporated.
The op amps are also supported by Microchip's Active Filter Demo Board Kit (part # MCP6XXXDM-FLTR, $65.00) and MCP6XXX evaluation boards (part #s MCP6XXXEV-AMP1, MCP6XXXEV-AMP2, MCP6XXXEV-AMP3, MCP6XXXEV-AMP4, respectively). All four of these boards are priced at $30.00 each and can be purchased at microchipDIRECT (http://www.microchip.com/get/XJ8S), today.
Packaging, Pricing & Availability
Part Number Package Option(s) 10k-unit Quantity Pricing MCP6401/1U/1R 5-pin SC-70, SOT-23 $0.26 each MCP6402 8-pin SOIC, 2 mm x 3 mm TDFN $0.32 each MCP6404 14-pin SOIC, TSSOP $0.43 each
Samples are available today at http://www.microchip.com/get/1R9R. Volume-production quantities can be purchased today at http://www.microchip.com/get/XJ8S. For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's Web site at http://www.microchip.com/get/X781.
About Microchip Technology
Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller, analog and Flash-IP solutions, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support, along with dependable delivery and quality. For more information, visit the Microchip Web site (http://www.microchip.com/get/LMTJ).
Note: The Microchip name and logo, and PIC are registered trademarks of Microchip Technology Incorporated in the U.S.A., and other countries. All other trademarks mentioned herein are the property of their respective companies.
High-res Photo and Block Diagram available through editorial contact or Flickr (feel free to publish):
Photo http://www.microchip.com/get/8M7V
Block Diagram http://www.microchip.com/get/MM4X
Tags / Keywords: Microchip, MCHP, PIC, microcontroller, MCU, low power, op amps, operational amplifier, MCP6XXX, MCP6401, MCP6402, MCP6404
RSS Feed for Microchip Product News: http://www.microchip.com/get/RQDG
    Source: Microchip Technology Inc.
    	Released July 27, 2010