Digital-to-Analog Converters from Microchip Enable Resolution, Output and Voltage-Reference Selection Flexibility

Single- and Dual-Output, 8-/10-bit Digital-to-Analog Converters (DACs) Feature Internal and External Voltage-Reference Options

CHANDLER, Ariz.--(BUSINESS WIRE)-- Microchip Technology Inc. (NASDAQ: MCHP), a leading provider of microcontroller and analog semiconductors, today announced the MCP4801/2, MCP4811/2 (MCP48XX) and MCP4901/2, MCP4911/2 (MCP49XX) Digital-to-Analog Converters (DACs). The new products expand the Company's portfolio of DACs with single- and dual-channel 8- and 10-bit devices featuring an SPI communication interface, as well as internal and external voltage-reference options. The MCP48XX family has an internal voltage reference, while the MCP49XX family accepts an external voltage reference. These DACs are appropriate for applications in the consumer (e.g., home appliances, LCD displays, computer peripherals); industrial (e.g., control systems, motor control, metering); and medical markets (e.g., ultrasound, ECG, sensor calibration), among others.

Because the MCP48XX and MCP49XX DACs offer both 8- and 10-bit resolution, designers can select the resolution needed for different applications. Additionally, having an integrated voltage reference reduces cost and space, while the external pin provides further design flexibility. Availability in small packages also saves space and makes the DACs easy to use.

"The expansion of our DAC portfolio brings greater competitive solutions to the market," said Bryan J. Liddiard, vice president of marketing with Microchip's Analog and Interface Products Division. "The availability of both 8- and 10-bit devices allows for the most cost-effective design."

"Designers often request more flexibility with regard to DAC resolution in their applications," said Jefferay Lawton, product marketing manager, Analog and Interface Products Division. "With the MCP48XX and MCP49XX families, designers can customize the resolution, number of outputs and voltage reference for each application."

Packaging, Pricing & Availability

The following table summarizes the MCP48XX and MCP49XX packaging and pricing options. Samples and volume-production quantities can be ordered today at http://www.microchip.com/get/JFFV and http://www.microchip.com/get/9LCU, respectively. For further information, contact any Microchip sales representative or authorized worldwide distributor, or visit Microchip's website at http://www.microchip.com/get/S7D1.


Product   Package Options                           10k-Unit Quantity Pricing

MCP4801   8-pin 2 mm x 3 mm DFN, MSOP, PDIP, SOIC   $0.81 each

MCP4811   8-pin 2 mm x 3 mm DFN, MSOP, PDIP, SOIC   $1.16 each

MCP4802   8-pin MSOP, PDIP, SOIC                    $1.06 each

MCP4812   8-pin MSOP, PDIP, SOIC                    $1.51 each

MCP4901   8-pin 2 mm x 3 mm DFN, MSOP, PDIP, SOIC   $0.69 each

MCP4911   8-pin 2 mm x 3 mm DFN, MSOP, PDIP, SOIC   $0.99 each

MCP4902   14-pin PDIP, SOIC                         $0.92 each

MCP4912   14-pin PDIP, SOIC, TSSOP                  $1.31 each



About Microchip Technology

Microchip Technology Inc. (NASDAQ: MCHP) is a leading provider of microcontroller and analog semiconductors, providing low-risk product development, lower total system cost and faster time to market for thousands of diverse customer applications worldwide. Headquartered in Chandler, Ariz., Microchip offers outstanding technical support along with dependable delivery and quality. For more information, visit the Microchip website at http://www.microchip.com/get/3MX6.

Note: The Microchip name and logo are registered trademarks of Microchip Technology Incorporated in the U.S.A. and other countries. All other trademarks mentioned herein are the property of their respective companies.

High-res Photo and Block Diagram available through editorial contact or Flickr (feel free to publish):

Photo: http://www.microchip.com/get/LAMU

Block Diagram: http://www.microchip.com/get/HVMM

Tags / Keywords: Microchip, MCHP, PIC, analog, DAC, digital-to-analog converter, MCP4801, MCP4811, MCP4802, MCP4812, MCP4901, MCP4911, MCP4902, MCP4912

RSS Feed for Microchip Product News: http://www.microchip.com/get/F9CL


    Source: Microchip Technology Inc.